<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX 8M Plus Yocto Image Bitbaking</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1500285#M193388</link>
    <description>&lt;P&gt;I could do the process successfully. The problem was bad internet connection, I brought pc to home and bitbake process completed. I could place sd card image to sd card and now I can run iMX board via SD Card. Thanks a lot.&lt;/P&gt;</description>
    <pubDate>Wed, 03 Aug 2022 12:51:09 GMT</pubDate>
    <dc:creator>fozen</dc:creator>
    <dc:date>2022-08-03T12:51:09Z</dc:date>
    <item>
      <title>i.MX 8M Plus Yocto Image Bitbaking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1469845#M191217</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I have i.MX 8M Plus EVK Board and I don't know anything about linux environment. I have started to read "i.MX Yocto Project User's Guide", "i.MX Linux® User's Guide" and "Freescale Yocto Project Tutorial" pdf files. I have a Ubuntu Machine (22.04) and sd card (32 GB) with sd card reader. I want to boot my EVK Board from sd card. I have started with&amp;nbsp;"i.MX Yocto Project User's Guide" at first and I stuck bitbaking part of the document. After I write "$ bitbake imx-image-multimedia" command it starts bitbaking, I face with some errors. I don't know it is okay or not but I want to continue to processes. My sd card is empty and when I want to write "$ sudo dd if=&amp;lt;image name&amp;gt;.wic of=/dev/sdx bs=1M &amp;amp;&amp;amp; sync" command I see that I need a wic extension document. I search it with find command but there is not any wic file.&lt;BR /&gt;&lt;BR /&gt;I thougt that's reason is faults as I mentioned above. Could you help me to have wic file. I add fault's image.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 10:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1469845#M191217</guid>
      <dc:creator>fozen</dc:creator>
      <dc:date>2022-06-07T10:21:31Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus Yocto Image Bitbaking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1469975#M191227</link>
      <description>&lt;P&gt;Before worrying about how to put your image on the SD card, fix the issues first. If you don't fix the build you will have nothing to put on the card! In your photograph it shows the build failure, it fails to fetch certain packages. Make sure you have installed the host packages as describe here by QMiller&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX8-fatal-error-attr-xattr-h-No-such-file-or-directory/m-p/1466318#M190977" target="_self"&gt;https://community.nxp.com/t5/i-MX-Processors/IMX8-fatal-error-attr-xattr-h-No-such-file-or-directory/m-p/1466318#M190977&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also for your first time try using a smaller image, like a core-image-minimum or core-image-base (or imx-image-xxx depending on your document)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 12:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1469975#M191227</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-06-07T12:01:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus Yocto Image Bitbaking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1470561#M191272</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200765"&gt;@fozen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The first task to fetch source file is failed. Firstly You need to make sure that you can access to these links for source file to fetch based on your local network.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As for the wic files to flash SD card. You will see it under this directory ./&amp;lt;your build directory&amp;gt;/tmp/deploy/images/../*.wic.bz2, If the whole build with success.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 09:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1470561#M191272</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2022-06-08T09:41:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus Yocto Image Bitbaking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1472001#M191350</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I have also updated and downloaded host packages except below. As I wrote before I use 22.04 Ubuntu version and it seems there is no package support for them.&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;E: Unable to locate package pylint3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;E: Unable to locate package lz4c&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;E: Unable to locate package pzstd&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;E: Package 'python' has no installation candidate&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;I have pylint instead of pylint3. I could not load python&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jun 2022 05:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1472001#M191350</guid>
      <dc:creator>fozen</dc:creator>
      <dc:date>2022-06-10T05:50:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus Yocto Image Bitbaking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1472087#M191355</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is getting a little out of the forum's point and more Ubuntu packaging issues; are you on a native machine or VM? Only thing I can suggest is you look at each error as an individual task and solve each one separately. It can take quite a while and lots of googling to crack such issues. If you're new to the Linux environment it can be quite challenging but we've all been there!&lt;/P&gt;&lt;P&gt;Here's a couple of links for the lz4c&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://installati.one/ubuntu/20.04/lz4/" target="_self"&gt;https://installati.one/ubuntu/20.04/lz4/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Locate package issues&lt;/P&gt;&lt;P&gt;&lt;A href="https://askubuntu.com/questions/378558/unable-to-locate-package-while-trying-to-install-packages-with-apt" target="_self"&gt;https://askubuntu.com/questions/378558/unable-to-locate-package-while-trying-to-install-packages-with-apt&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, you need to use/fix python3 packages where required.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edit: The&amp;nbsp;31 March 2022 imx8 Yocto project user guides suggests 20.04 or later; I've been using Yocto for around 8 years for work on a number of devices and have found the later versions of Ubuntu (post document date) can give build headaches. A few times I've had to roll back my build machine version (imx7sabresd for example) to the one stated in the doc.&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jun 2022 08:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1472087#M191355</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-06-10T08:39:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus Yocto Image Bitbaking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1492218#M192744</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192970"&gt;@Harvey021&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;There is an update on my side. I changed OS, now I use Ubuntu 20.04 LTS. I have not faced with package problem. There is a problem on just one task while bitbaking. I have tried many many times but linux-imx-5.15.32+gitAUTONIC+fa6c316859-r0 do_fetch task was never completed. What could be the reason ? Some guys say weak internet connection but I want to be sure on this topic. Is it possible to change 5.15.32 to different one ? I don't know if it works or not, I am just asking.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 06:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1492218#M192744</guid>
      <dc:creator>fozen</dc:creator>
      <dc:date>2022-07-20T06:51:19Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus Yocto Image Bitbaking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1492273#M192752</link>
      <description>&lt;P&gt;As a test you could try rolling back. In the doc you'll see the following repo set up:&amp;nbsp;&lt;/P&gt;&lt;P&gt;mkdir imx-yocto-bsp&lt;BR /&gt;cd imx-yocto-bsp&lt;BR /&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="_blank" rel="noopener"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt;&amp;nbsp;-b imx-linux-honister -m imx-5.15.5-.0.0.xml&lt;BR /&gt;repo sync&lt;/P&gt;&lt;P&gt;Change these options to select different flavours/kernels:&amp;nbsp;-b imx-linux-honister&amp;nbsp; and&amp;nbsp; -m imx-5.15.5-.0.0.xml&lt;/P&gt;&lt;P&gt;In your attached image your kernel was 5.15, did you move away from that build? You could try that again on your new 20.04 machine. According to docs.yoctoproject there are a few kernel options (and one not listed in the removed list obviously). You don't have to specify the -m kernel option if you can't find any references to the xml file, it will just use the default.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN class=""&gt;linux-yocto&lt;/SPAN&gt;: removed version 5.4 recipes (5.14 and 5.10 still provided)&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;A href="https://docs.yoctoproject.org/migration-guides/release-3.4.html" target="_self"&gt;https://docs.yoctoproject.org/migration-guides/release-3.4.html&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 08:02:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1492273#M192752</guid>
      <dc:creator>edwardtyrrell</dc:creator>
      <dc:date>2022-07-20T08:02:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus Yocto Image Bitbaking</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1500285#M193388</link>
      <description>&lt;P&gt;I could do the process successfully. The problem was bad internet connection, I brought pc to home and bitbake process completed. I could place sd card image to sd card and now I can run iMX board via SD Card. Thanks a lot.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 12:51:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-Yocto-Image-Bitbaking/m-p/1500285#M193388</guid>
      <dc:creator>fozen</dc:creator>
      <dc:date>2022-08-03T12:51:09Z</dc:date>
    </item>
  </channel>
</rss>