<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Network config in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Network-config/m-p/1500111#M193376</link>
    <description>&lt;P&gt;If your board is boot up in Linux, then you could configure the network setting same as other Linux system. Or i think you could add the setting in the start up script. You may get more examples in google search.&lt;/P&gt;</description>
    <pubDate>Wed, 03 Aug 2022 08:40:13 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2022-08-03T08:40:13Z</dc:date>
    <item>
      <title>Network config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Network-config/m-p/1493145#M192809</link>
      <description>&lt;P&gt;I want to set the network configuration of my evk board for ethernet routing.&lt;/P&gt;&lt;P&gt;I know it can be changed by 'route' command,&lt;/P&gt;&lt;P&gt;but I want to apply the configuration through the config file so that the my-config remained permanently.&lt;/P&gt;&lt;P&gt;But I don't know where could I found the file for network configuration&lt;/P&gt;&lt;P&gt;such as '/etc/sysconfig/network' or '/etc/network/interfaces' of other Linux system.&lt;/P&gt;&lt;P&gt;I'm using imx8mq-evk board now.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 07:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Network-config/m-p/1493145#M192809</guid>
      <dc:creator>CHOIzee</dc:creator>
      <dc:date>2022-07-21T07:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: Network config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Network-config/m-p/1500111#M193376</link>
      <description>&lt;P&gt;If your board is boot up in Linux, then you could configure the network setting same as other Linux system. Or i think you could add the setting in the start up script. You may get more examples in google search.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 08:40:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Network-config/m-p/1500111#M193376</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-08-03T08:40:13Z</dc:date>
    </item>
  </channel>
</rss>