<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX 8M Mini - GPIO current capability in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-GPIO-current-capability/m-p/1499789#M193339</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; First think, all the pin are categorised into GPIO label(From table 7) and digital I/O are categorised into GPIO pre-driver (PVCC). It's operations range from 1.65 to 1.95 volts 3mA. But table no21 mentioned,&amp;nbsp; all the peripheral which is classified in table 7&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Aug 2022 19:14:39 GMT</pubDate>
    <dc:creator>KalaimaniArumugamdev</dc:creator>
    <dc:date>2022-08-02T19:14:39Z</dc:date>
    <item>
      <title>i.MX 8M Mini - GPIO current capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-GPIO-current-capability/m-p/1499773#M193335</link>
      <description>&lt;P&gt;I need to know how much current the GPIO can source and sink.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example, pins P108 and P109 (GPIO_0, GPIO_1).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The datasheet says the output voltage of the pins was tested at 9.6 mA and held 1.8V (section 3.5, table 21).&lt;/P&gt;&lt;P&gt;But then I see the data sheet says the PVCCx1P8 says 3mA max but I'm not sure what "GPIO pre driver" means.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 18:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-GPIO-current-capability/m-p/1499773#M193335</guid>
      <dc:creator>RobotDR84</dc:creator>
      <dc:date>2022-08-02T18:00:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini - GPIO current capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-GPIO-current-capability/m-p/1499789#M193339</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; First think, all the pin are categorised into GPIO label(From table 7) and digital I/O are categorised into GPIO pre-driver (PVCC). It's operations range from 1.65 to 1.95 volts 3mA. But table no21 mentioned,&amp;nbsp; all the peripheral which is classified in table 7&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 19:14:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-GPIO-current-capability/m-p/1499789#M193339</guid>
      <dc:creator>KalaimaniArumugamdev</dc:creator>
      <dc:date>2022-08-02T19:14:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini - GPIO current capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-GPIO-current-capability/m-p/1499792#M193340</link>
      <description>&lt;P&gt;Thank you for your response, but I am still a bit unsure of what you're saying.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 19:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-GPIO-current-capability/m-p/1499792#M193340</guid>
      <dc:creator>RobotDR84</dc:creator>
      <dc:date>2022-08-02T19:20:26Z</dc:date>
    </item>
  </channel>
</rss>