<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic cockpit recipe in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/cockpit-recipe/m-p/1499748#M193330</link>
    <description>&lt;P&gt;I am trying to add cockpit to my image.&lt;/P&gt;&lt;P&gt;cockpit is a webserver utility able to do linux system configuration from a web-browser. for example change IP address.&lt;/P&gt;&lt;P&gt;the recipe is located under:&lt;/P&gt;&lt;P&gt;meta-openembedded/meta-webserver/recipes-webadmin/cockpit/cockpit_220.bb&lt;/P&gt;&lt;P&gt;I have added&amp;nbsp;meta-openembedded/meta-webserver to bblayers.conf file&lt;/P&gt;&lt;P&gt;added cockpit to CORE_IMAGE_EXTRA_INSTALL in local.conf&lt;/P&gt;&lt;P&gt;the bitbake of my image is done and the image is burned.&lt;/P&gt;&lt;P&gt;I cannot see most of the installed files when running the image on target. cockpit service in not running.&lt;/P&gt;&lt;P&gt;have someone tried to do this with IMX8 and can help ?&lt;/P&gt;</description>
    <pubDate>Tue, 02 Aug 2022 16:58:25 GMT</pubDate>
    <dc:creator>razriel</dc:creator>
    <dc:date>2022-08-02T16:58:25Z</dc:date>
    <item>
      <title>cockpit recipe</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cockpit-recipe/m-p/1499748#M193330</link>
      <description>&lt;P&gt;I am trying to add cockpit to my image.&lt;/P&gt;&lt;P&gt;cockpit is a webserver utility able to do linux system configuration from a web-browser. for example change IP address.&lt;/P&gt;&lt;P&gt;the recipe is located under:&lt;/P&gt;&lt;P&gt;meta-openembedded/meta-webserver/recipes-webadmin/cockpit/cockpit_220.bb&lt;/P&gt;&lt;P&gt;I have added&amp;nbsp;meta-openembedded/meta-webserver to bblayers.conf file&lt;/P&gt;&lt;P&gt;added cockpit to CORE_IMAGE_EXTRA_INSTALL in local.conf&lt;/P&gt;&lt;P&gt;the bitbake of my image is done and the image is burned.&lt;/P&gt;&lt;P&gt;I cannot see most of the installed files when running the image on target. cockpit service in not running.&lt;/P&gt;&lt;P&gt;have someone tried to do this with IMX8 and can help ?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 16:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cockpit-recipe/m-p/1499748#M193330</guid>
      <dc:creator>razriel</dc:creator>
      <dc:date>2022-08-02T16:58:25Z</dc:date>
    </item>
    <item>
      <title>Re: cockpit recipe</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cockpit-recipe/m-p/1508232#M193992</link>
      <description>&lt;P&gt;it worked for me after adding some more packages to local.conf file:&lt;/P&gt;&lt;P&gt;CORE_IMAGE_EXTRA_INSTALL += " cockpit \&lt;BR /&gt;cockpit-pcp \&lt;BR /&gt;cockpit-tuned \&lt;BR /&gt;cockpit-shell \&lt;BR /&gt;cockpit-systemd \&lt;BR /&gt;cockpit-users \&lt;BR /&gt;cockpit-kdump \&lt;BR /&gt;cockpit-sosreport \&lt;BR /&gt;cockpit-networkmanager \&lt;BR /&gt;cockpit-machines \&lt;BR /&gt;cockpit-selinux \&lt;BR /&gt;cockpit-playground \&lt;BR /&gt;cockpit-docker \&lt;BR /&gt;cockpit-dashboard \&lt;BR /&gt;cockpit-bridge \&lt;BR /&gt;cockpit-ws \&lt;BR /&gt;cockpit-desktop \&lt;BR /&gt;"&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 11:50:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cockpit-recipe/m-p/1508232#M193992</guid>
      <dc:creator>razriel</dc:creator>
      <dc:date>2022-08-18T11:50:40Z</dc:date>
    </item>
    <item>
      <title>Re: cockpit recipe</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cockpit-recipe/m-p/1848439#M222614</link>
      <description>&lt;P&gt;Any chance you found a fix for this?&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 19:34:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cockpit-recipe/m-p/1848439#M222614</guid>
      <dc:creator>andrewLinux</dc:creator>
      <dc:date>2024-04-16T19:34:10Z</dc:date>
    </item>
  </channel>
</rss>