<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QXcbIntegration-Cannot-create-platform-OpenGL-context-neither/m-p/1498566#M193248</link>
    <description>&lt;P&gt;Hi Sir&lt;/P&gt;&lt;P&gt;I use the iMX8QM EVK and follow imx-yocto-L4.14.98_2.0.0_ga user'guide.&lt;/P&gt;&lt;P&gt;I can success to use SV3D-1.1 sample.&lt;/P&gt;&lt;P&gt;Now，I want to use QT to design the UI, so I use fsl-image-qt5-validation-imx to support QT5.&lt;/P&gt;&lt;P&gt;and I can use cross compile to test the qt project on iMX8 EVK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;But, when I use the OpenGL like QOpenGLWidget or QGLWidget on QT project, the terminal will show&lt;/P&gt;&lt;P&gt;as below:&lt;/P&gt;&lt;P&gt;"QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled'&lt;/P&gt;&lt;P&gt;I check the fsl-image-qt5-validation-imx image QT5 example, the path is /usr/share/qt5/examples/opengl/hellogl2/./hellogl2.&lt;/P&gt;&lt;P&gt;It has the same problem.&lt;/P&gt;&lt;P&gt;Please kindly to help me to solved this question&lt;/P&gt;&lt;P&gt;thanks a lot&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 01 Aug 2022 06:58:28 GMT</pubDate>
    <dc:creator>alonghong</dc:creator>
    <dc:date>2022-08-01T06:58:28Z</dc:date>
    <item>
      <title>QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QXcbIntegration-Cannot-create-platform-OpenGL-context-neither/m-p/1498566#M193248</link>
      <description>&lt;P&gt;Hi Sir&lt;/P&gt;&lt;P&gt;I use the iMX8QM EVK and follow imx-yocto-L4.14.98_2.0.0_ga user'guide.&lt;/P&gt;&lt;P&gt;I can success to use SV3D-1.1 sample.&lt;/P&gt;&lt;P&gt;Now，I want to use QT to design the UI, so I use fsl-image-qt5-validation-imx to support QT5.&lt;/P&gt;&lt;P&gt;and I can use cross compile to test the qt project on iMX8 EVK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;But, when I use the OpenGL like QOpenGLWidget or QGLWidget on QT project, the terminal will show&lt;/P&gt;&lt;P&gt;as below:&lt;/P&gt;&lt;P&gt;"QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled'&lt;/P&gt;&lt;P&gt;I check the fsl-image-qt5-validation-imx image QT5 example, the path is /usr/share/qt5/examples/opengl/hellogl2/./hellogl2.&lt;/P&gt;&lt;P&gt;It has the same problem.&lt;/P&gt;&lt;P&gt;Please kindly to help me to solved this question&lt;/P&gt;&lt;P&gt;thanks a lot&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 06:58:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QXcbIntegration-Cannot-create-platform-OpenGL-context-neither/m-p/1498566#M193248</guid>
      <dc:creator>alonghong</dc:creator>
      <dc:date>2022-08-01T06:58:28Z</dc:date>
    </item>
    <item>
      <title>Re: QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QXcbIntegration-Cannot-create-platform-OpenGL-context-neither/m-p/1499627#M193321</link>
      <description>&lt;P&gt;Hello alonghong,&lt;/P&gt;
&lt;P&gt;You need to use the L5.4.70 at least to use OpenGL with QT.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 13:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QXcbIntegration-Cannot-create-platform-OpenGL-context-neither/m-p/1499627#M193321</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-08-02T13:42:52Z</dc:date>
    </item>
    <item>
      <title>回复： QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QXcbIntegration-Cannot-create-platform-OpenGL-context-neither/m-p/1500803#M193415</link>
      <description>&lt;P&gt;Hi Bio_TICFSL&lt;/P&gt;&lt;P&gt;I solved this issue, the solution is when I&amp;nbsp;execute my test application, I need to key ./test -platform wayland-egl.&lt;/P&gt;&lt;P&gt;and then the application is work.&lt;/P&gt;&lt;P&gt;but I find another question is when I move the yuv data to&amp;nbsp; y , u , v array and use the opengl to paint image.&lt;/P&gt;&lt;P&gt;the action spend a lot of time to complete. I don't know what's happened.&lt;/P&gt;&lt;P&gt;please kindly to help me solve this question&lt;/P&gt;&lt;P&gt;thanks a lot&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Aug 2022 06:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QXcbIntegration-Cannot-create-platform-OpenGL-context-neither/m-p/1500803#M193415</guid>
      <dc:creator>alonghong</dc:creator>
      <dc:date>2022-08-04T06:05:37Z</dc:date>
    </item>
  </channel>
</rss>