<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックglfw apps crash when used with wlroots based compositor</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/glfw-apps-crash-when-used-with-wlroots-based-compositor/m-p/1496531#M193114</link>
    <description>&lt;P&gt;All glfw applications seems to crash at start-up when launched with a wlroots based compositor (sway or cage have the same behavior). We tested our custom application and a GLES3 example (FractalShader) in the imx gpu sdk.&lt;/P&gt;&lt;P&gt;Weston-terminal work well when launched with cage and our app/the SDK example work when launched with weston. The problem seems to only occur when both glfw and wlroots are used together.&lt;/P&gt;&lt;P&gt;Please find attached the valgrind log of a glfw application compiled with debug symbols.&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jul 2022 16:28:13 GMT</pubDate>
    <dc:creator>alamache</dc:creator>
    <dc:date>2022-07-27T16:28:13Z</dc:date>
    <item>
      <title>glfw apps crash when used with wlroots based compositor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/glfw-apps-crash-when-used-with-wlroots-based-compositor/m-p/1496531#M193114</link>
      <description>&lt;P&gt;All glfw applications seems to crash at start-up when launched with a wlroots based compositor (sway or cage have the same behavior). We tested our custom application and a GLES3 example (FractalShader) in the imx gpu sdk.&lt;/P&gt;&lt;P&gt;Weston-terminal work well when launched with cage and our app/the SDK example work when launched with weston. The problem seems to only occur when both glfw and wlroots are used together.&lt;/P&gt;&lt;P&gt;Please find attached the valgrind log of a glfw application compiled with debug symbols.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 16:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/glfw-apps-crash-when-used-with-wlroots-based-compositor/m-p/1496531#M193114</guid>
      <dc:creator>alamache</dc:creator>
      <dc:date>2022-07-27T16:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: glfw apps crash when used with wlroots based compositor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/glfw-apps-crash-when-used-with-wlroots-based-compositor/m-p/1507899#M193971</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204266"&gt;@alamache&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which BSP and board you are using?&lt;/P&gt;</description>
      <pubDate>Thu, 18 Aug 2022 02:27:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/glfw-apps-crash-when-used-with-wlroots-based-compositor/m-p/1507899#M193971</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-08-18T02:27:40Z</dc:date>
    </item>
    <item>
      <title>Re: glfw apps crash when used with wlroots based compositor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/glfw-apps-crash-when-used-with-wlroots-based-compositor/m-p/1513910#M194454</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;we're currently using an imx8mplus with an kirkstone yocto SDK and the non community BSP&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 12:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/glfw-apps-crash-when-used-with-wlroots-based-compositor/m-p/1513910#M194454</guid>
      <dc:creator>alamache</dc:creator>
      <dc:date>2022-08-30T12:19:09Z</dc:date>
    </item>
  </channel>
</rss>