<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1061 falied to power up dap in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-falied-to-power-up-dap/m-p/1495460#M193036</link>
    <description>&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Customer had used Low Power Idle mode, the source of wake-up was GPIO interrupt input.&lt;BR /&gt;Now we cannot know whether these boards will crash again or not. This problem is difficult to appear, maybe for days or months. These boards electrical specifications&amp;nbsp;are same to other correct boards. We want to know what's the state of RT1061 when the VCC_SOC_IN be 1.27V. I supposed to MCU had been waked up, and run into full speed clock mode. But I cannot understand that why Jlink failed to connect the MCU.&lt;/P&gt;</description>
    <pubDate>Tue, 26 Jul 2022 08:58:18 GMT</pubDate>
    <dc:creator>cyesman</dc:creator>
    <dc:date>2022-07-26T08:58:18Z</dc:date>
    <item>
      <title>RT1061 falied to power up dap</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-falied-to-power-up-dap/m-p/1494939#M192983</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Customer had applied the RT1061 into production for months . Now several boards seems to be unnormally. The VCC_SOC_IN was 1.275V, Jlink cannot connect the core via to SWD line(Jlink found SWD-DP with ID 0x0BD11477 Failed to power up DAP), the code didn't run up.&lt;BR /&gt;&lt;/SPAN&gt;When reset the RT1061, it worked well as usual. Hardly to recover this issue.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 16:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-falied-to-power-up-dap/m-p/1494939#M192983</guid>
      <dc:creator>cyesman</dc:creator>
      <dc:date>2022-07-25T16:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 falied to power up dap</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-falied-to-power-up-dap/m-p/1495391#M193030</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;According to the above statement, some boards will crash after running for a period of time, further, the Jlink also fails to connect them.&lt;BR /&gt;However, it will run well again after repower-up.&lt;BR /&gt;If my understanding is right, I'd like to know if these boards will crash again, do these boards have some different electrical specifications versus correct boards? &lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 08:05:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-falied-to-power-up-dap/m-p/1495391#M193030</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-07-26T08:05:38Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 falied to power up dap</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-falied-to-power-up-dap/m-p/1495460#M193036</link>
      <description>&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Customer had used Low Power Idle mode, the source of wake-up was GPIO interrupt input.&lt;BR /&gt;Now we cannot know whether these boards will crash again or not. This problem is difficult to appear, maybe for days or months. These boards electrical specifications&amp;nbsp;are same to other correct boards. We want to know what's the state of RT1061 when the VCC_SOC_IN be 1.27V. I supposed to MCU had been waked up, and run into full speed clock mode. But I cannot understand that why Jlink failed to connect the MCU.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 08:58:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-falied-to-power-up-dap/m-p/1495460#M193036</guid>
      <dc:creator>cyesman</dc:creator>
      <dc:date>2022-07-26T08:58:18Z</dc:date>
    </item>
  </channel>
</rss>