<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Standalone Boot loader for imxrt1060</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1492630#M192780</link>
    <description>&lt;P&gt;Can someone please reply to this?&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jul 2022 17:21:54 GMT</pubDate>
    <dc:creator>palak_shah1</dc:creator>
    <dc:date>2022-07-20T17:21:54Z</dc:date>
    <item>
      <title>Standalone Boot loader for imxrt1060</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1491975#M192720</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have an imxrt1060 based custom board. We are running our own application on it so far and its OK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Either I use a jtag to download the code or flash the code on the QSPI flash using MCU boot utility.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, there is a need to add a boot loader. I have seen the SDK examples - evkimxrt_flashloader and imxrt_mcuboot_opensource. I have also looked at the SBL and SFW source code, but these are huge sources and has a lot of functionality.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am looking for a stand alone boot loader which is its own application that i can flash on the QSPI flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any example or code available that I can use or look at?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Palak&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jul 2022 18:14:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1491975#M192720</guid>
      <dc:creator>palak_shah1</dc:creator>
      <dc:date>2022-07-19T18:14:59Z</dc:date>
    </item>
    <item>
      <title>Re: Standalone Boot loader for imxrt1060</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1492630#M192780</link>
      <description>&lt;P&gt;Can someone please reply to this?&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 17:21:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1492630#M192780</guid>
      <dc:creator>palak_shah1</dc:creator>
      <dc:date>2022-07-20T17:21:54Z</dc:date>
    </item>
    <item>
      <title>Re: Standalone Boot loader for imxrt1060</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1494108#M192878</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I really want to know if we have any stand alone boot loader examples for imxrt1060 based. Any input is appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Palak&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jul 2022 14:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1494108#M192878</guid>
      <dc:creator>palak_shah1</dc:creator>
      <dc:date>2022-07-22T14:49:56Z</dc:date>
    </item>
    <item>
      <title>Re: Standalone Boot loader for imxrt1060</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1497565#M193178</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/140741"&gt;@palak_shah1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think that you could refer to the&amp;nbsp;&amp;nbsp;AN12604 Implement second bootloader on i.MXRT10xx series (i.MX RT1050, i.MX RT1020, and i.MX RT1060 are covered in the app note)&lt;/P&gt;
&lt;P&gt;This application note provides information about the basic elements to implement a secondary bootloader. The software for this application&amp;nbsp; note is here&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note-software/AN12604SW.zip" target="_self"&gt;AN12604 software&amp;nbsp;&amp;nbsp;&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do not hesitate to let me know if there is anything else we should discuss.&lt;/P&gt;
&lt;P&gt;Many thanks for your patience.&lt;/P&gt;
&lt;P&gt;Diego.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jul 2022 23:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Standalone-Boot-loader-for-imxrt1060/m-p/1497565#M193178</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2022-07-28T23:00:27Z</dc:date>
    </item>
  </channel>
</rss>