<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX8MP NPU inference source code</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1492337#M192759</link>
    <description>&lt;P&gt;I agree the high level software sources are easy to find (I mentionned tflite is OK). It is the low level software sources I'm trying to find : NNRT, OVXLIB and the OpenVX driver.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jul 2022 09:31:15 GMT</pubDate>
    <dc:creator>mbrundler</dc:creator>
    <dc:date>2022-07-20T09:31:15Z</dc:date>
    <item>
      <title>I.MX8MP NPU inference source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1488150#M192433</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have built a disk image and an SDK for an I/MX8M Plus target, using yocto from a&amp;nbsp;imx-5.10.35-2.0.0.xml manifest.&lt;/P&gt;&lt;P&gt;We have developped an inference sw based on the 'label_image' example, that executes inferences targeting the NPU (VIP8000Nano), using the tflite / NNAPI sw stack.&lt;/P&gt;&lt;P&gt;Information from the I.MX_Machine_learning _UG lists the sw layers involved in NPU inference and we would like to see the source code of those layers (tflite, NNAPI delegate, NNAPI, nn_runtime,&amp;nbsp; OVXLIB and OpenVX driver).&lt;/P&gt;&lt;P&gt;For the components built by yocto/bitbake from sources, the source files should be left sowewhere in the yocto work tree, but I actually found only the tflite sources.&lt;/P&gt;&lt;P&gt;For&amp;nbsp; the other layers, are the sources availaible and where (codeaurora, a github, ...) ?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 13:00:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1488150#M192433</guid>
      <dc:creator>mbrundler</dc:creator>
      <dc:date>2022-07-12T13:00:49Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MP NPU inference source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1488447#M192454</link>
      <description>&lt;P&gt;you can search from here, for example tensorflow:&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://source.codeaurora.org/external/imx/tensorflow-imx/tree/?h=lf-5.10.72_2.2.0&amp;quot;" target="_blank"&gt;https://source.codeaurora.org/external/imx/tensorflow-imx/tree/?h=lf-5.10.72_2.2.0"&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;or &lt;A title="onnxruntime-imx" href="https://source.codeaurora.org/external/imx/onnxruntime-imx/" target="_blank"&gt;onnxruntime&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://source.codeaurora.org/external/imx/onnxruntime-imx/tree/?h=lf-5.15.32_2.0.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/onnxruntime-imx/tree/?h=lf-5.15.32_2.0.0&lt;/A&gt;"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 03:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1488447#M192454</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-07-13T03:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MP NPU inference source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1492337#M192759</link>
      <description>&lt;P&gt;I agree the high level software sources are easy to find (I mentionned tflite is OK). It is the low level software sources I'm trying to find : NNRT, OVXLIB and the OpenVX driver.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 09:31:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1492337#M192759</guid>
      <dc:creator>mbrundler</dc:creator>
      <dc:date>2022-07-20T09:31:15Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MP NPU inference source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1499280#M193289</link>
      <description>&lt;P&gt;I don't think we can share this GPU driver in this public community&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 06:32:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-NPU-inference-source-code/m-p/1499280#M193289</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-08-02T06:32:15Z</dc:date>
    </item>
  </channel>
</rss>