<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8MP check NPU usage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1492297#M192756</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp;IMX8MP with the system Yocto Linux. I'd like to check&amp;nbsp;NPU usage, such as the "%CPU" from the command "top". I have noticed the description like "&lt;SPAN&gt;Arm® Cortex®-A53 with an integrated NPU".&amp;nbsp;Does it mean that the NPU is integrated into the CPU, so it can't be checked alone?&amp;nbsp;If so, does the CPU usage also include the usage of the integrated NPU?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jul 2022 08:46:38 GMT</pubDate>
    <dc:creator>Eric97</dc:creator>
    <dc:date>2022-07-20T08:46:38Z</dc:date>
    <item>
      <title>IMX8MP check NPU usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1492297#M192756</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp;IMX8MP with the system Yocto Linux. I'd like to check&amp;nbsp;NPU usage, such as the "%CPU" from the command "top". I have noticed the description like "&lt;SPAN&gt;Arm® Cortex®-A53 with an integrated NPU".&amp;nbsp;Does it mean that the NPU is integrated into the CPU, so it can't be checked alone?&amp;nbsp;If so, does the CPU usage also include the usage of the integrated NPU?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 08:46:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1492297#M192756</guid>
      <dc:creator>Eric97</dc:creator>
      <dc:date>2022-07-20T08:46:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP check NPU usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1492519#M192771</link>
      <description>&lt;P&gt;Hello Jichen,&lt;/P&gt;
&lt;P&gt;It can be checked but when you use one of the machine learning tools please check it:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MP-NPU-debug-and-fine-tune-application-note/ta-p/1444775" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MP-NPU-debug-and-fine-tune-application-note/ta-p/1444775&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 13:57:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1492519#M192771</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-07-20T13:57:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP check NPU usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1493264#M192817</link>
      <description>&lt;P&gt;Thanks a lot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;Using machine learning tools like NPU PROFILER, we can obtain the processing time of each operator on the NPU. What I need is to get the NPU usage in real time like&amp;nbsp;t&lt;SPAN&gt;he percentage of NPU that is being used by the process.&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;For example, using command "top", we can get the %CPU.&amp;nbsp;Can we get similar information for NPU?&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Jichen_vs_0-1658398045835.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/187400iE05157DC7A67D47E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Jichen_vs_0-1658398045835.png" alt="Jichen_vs_0-1658398045835.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Or does the CPU information we get include NPU? Because I see the&amp;nbsp;&lt;SPAN&gt;NPU is an integrated NPU in Arm® Cortex®-A53 CPU.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 10:11:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1493264#M192817</guid>
      <dc:creator>Eric97</dc:creator>
      <dc:date>2022-07-21T10:11:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP check NPU usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1769707#M216945</link>
      <description>&lt;P&gt;Did anyone found any solution, to see NPU utilization % realtime&lt;/P&gt;</description>
      <pubDate>Wed, 06 Dec 2023 10:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1769707#M216945</guid>
      <dc:creator>Hitesh_em</dc:creator>
      <dc:date>2023-12-06T10:15:29Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP check NPU usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1932109#M227314</link>
      <description>Any updates on that?</description>
      <pubDate>Wed, 14 Aug 2024 15:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-check-NPU-usage/m-p/1932109#M227314</guid>
      <dc:creator>ooper901</dc:creator>
      <dc:date>2024-08-14T15:15:52Z</dc:date>
    </item>
  </channel>
</rss>