<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCAN BUS iMX8QXP MEK in Android Automotive</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CAN-BUS-iMX8QXP-MEK-in-Android-Automotive/m-p/1492253#M192749</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I'm trying to use the can bus interfaces in Android Automotive but for now, isn't possible.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have enabled flexcan driver in the kernel configuration using menuconfig.&amp;nbsp;&lt;BR /&gt;After this, in the adb logcat, i see the vcan and can driver fet up in boot but anything about can0,can1 and can2.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;As I have seen in other forum posts, the can bus resources are assigned to the m4 processor. So I've tried to delete the m4 processor partition using a custom scfw but I haven't noticed any change.&lt;/P&gt;&lt;P&gt;In fact, I am making use of the android automotive mek_8q_car2 image and when I use the custom scfw without the m4 partition, I still see the power switch on the m4 processor when I understand that it should not be.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So my question is:&lt;/P&gt;&lt;P&gt;Is it possible to make use of CAN interfaces from cortex A in android automotive?&lt;/P&gt;&lt;P&gt;If this is not possible, Android Automotive could read the canbus data from the M4 processor and interpret it in the Cortex A.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jul 2022 07:32:04 GMT</pubDate>
    <dc:creator>esqui2002</dc:creator>
    <dc:date>2022-07-20T07:32:04Z</dc:date>
    <item>
      <title>CAN BUS iMX8QXP MEK in Android Automotive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-BUS-iMX8QXP-MEK-in-Android-Automotive/m-p/1492253#M192749</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I'm trying to use the can bus interfaces in Android Automotive but for now, isn't possible.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have enabled flexcan driver in the kernel configuration using menuconfig.&amp;nbsp;&lt;BR /&gt;After this, in the adb logcat, i see the vcan and can driver fet up in boot but anything about can0,can1 and can2.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;As I have seen in other forum posts, the can bus resources are assigned to the m4 processor. So I've tried to delete the m4 processor partition using a custom scfw but I haven't noticed any change.&lt;/P&gt;&lt;P&gt;In fact, I am making use of the android automotive mek_8q_car2 image and when I use the custom scfw without the m4 partition, I still see the power switch on the m4 processor when I understand that it should not be.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So my question is:&lt;/P&gt;&lt;P&gt;Is it possible to make use of CAN interfaces from cortex A in android automotive?&lt;/P&gt;&lt;P&gt;If this is not possible, Android Automotive could read the canbus data from the M4 processor and interpret it in the Cortex A.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 07:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-BUS-iMX8QXP-MEK-in-Android-Automotive/m-p/1492253#M192749</guid>
      <dc:creator>esqui2002</dc:creator>
      <dc:date>2022-07-20T07:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: CAN BUS iMX8QXP MEK in Android Automotive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-BUS-iMX8QXP-MEK-in-Android-Automotive/m-p/1500298#M193389</link>
      <description>&lt;P&gt;Hello esqui2002,&lt;/P&gt;
&lt;P&gt;A1. No, because CAN it's not implemented in android just for the M4.&lt;/P&gt;
&lt;P&gt;A2. Yes, you can send a message fro M4 to cortex A&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 13:22:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-BUS-iMX8QXP-MEK-in-Android-Automotive/m-p/1500298#M193389</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-08-03T13:22:21Z</dc:date>
    </item>
  </channel>
</rss>