<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Timeout error when flashing IMX8Mplus using UUU</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Timeout-error-when-flashing-IMX8Mplus-using-UUU/m-p/1491631#M192698</link>
    <description>&lt;P&gt;I built a custom board and used IMX8M plus processor. When the firmware team tried to upload the prebuilt image of the EVK dev board using UUU they encounter this issue:&lt;/P&gt;&lt;P&gt;Fail HID(W):LIBUSB_ERROR_TIMEOUT(1s)&lt;/P&gt;&lt;P&gt;There are a few differences between the custom board design and the EVK dev board, and the differences are:&lt;/P&gt;&lt;P&gt;1/ To upload the image I connected the Micro-b USB 2.0 directly to USB1 of IMX8M plus, whilst in the dev board the USB is connected to USB-to-Serial IC and then connected two UART signals to UART 2 and 4 of IMX8M plus&lt;/P&gt;&lt;P&gt;2/ DRAM:&lt;/P&gt;&lt;P&gt;We used 2GB LPDDR4 PN:MT53D512M32D2DS-053 AAT:D&lt;/P&gt;&lt;P&gt;Dev Board 6GB LPPDR4 PN:MT53E1536M32D4DT-046 WT:A&lt;/P&gt;&lt;P&gt;3/ Same PMIC&lt;/P&gt;&lt;P&gt;4/eMMC:&lt;/P&gt;&lt;P&gt;We used 8GB eMMC 5.1 PN:SDINBDG4-8G-XA&lt;/P&gt;&lt;P&gt;Dev Board 32GB eMMC5.1 PN:SDINBDG4-32G-I1&lt;/P&gt;&lt;P&gt;Any idea what seems to be the problem?&lt;/P&gt;</description>
    <pubDate>Tue, 19 Jul 2022 08:52:21 GMT</pubDate>
    <dc:creator>Talal</dc:creator>
    <dc:date>2022-07-19T08:52:21Z</dc:date>
    <item>
      <title>Timeout error when flashing IMX8Mplus using UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Timeout-error-when-flashing-IMX8Mplus-using-UUU/m-p/1491631#M192698</link>
      <description>&lt;P&gt;I built a custom board and used IMX8M plus processor. When the firmware team tried to upload the prebuilt image of the EVK dev board using UUU they encounter this issue:&lt;/P&gt;&lt;P&gt;Fail HID(W):LIBUSB_ERROR_TIMEOUT(1s)&lt;/P&gt;&lt;P&gt;There are a few differences between the custom board design and the EVK dev board, and the differences are:&lt;/P&gt;&lt;P&gt;1/ To upload the image I connected the Micro-b USB 2.0 directly to USB1 of IMX8M plus, whilst in the dev board the USB is connected to USB-to-Serial IC and then connected two UART signals to UART 2 and 4 of IMX8M plus&lt;/P&gt;&lt;P&gt;2/ DRAM:&lt;/P&gt;&lt;P&gt;We used 2GB LPDDR4 PN:MT53D512M32D2DS-053 AAT:D&lt;/P&gt;&lt;P&gt;Dev Board 6GB LPPDR4 PN:MT53E1536M32D4DT-046 WT:A&lt;/P&gt;&lt;P&gt;3/ Same PMIC&lt;/P&gt;&lt;P&gt;4/eMMC:&lt;/P&gt;&lt;P&gt;We used 8GB eMMC 5.1 PN:SDINBDG4-8G-XA&lt;/P&gt;&lt;P&gt;Dev Board 32GB eMMC5.1 PN:SDINBDG4-32G-I1&lt;/P&gt;&lt;P&gt;Any idea what seems to be the problem?&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jul 2022 08:52:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Timeout-error-when-flashing-IMX8Mplus-using-UUU/m-p/1491631#M192698</guid>
      <dc:creator>Talal</dc:creator>
      <dc:date>2022-07-19T08:52:21Z</dc:date>
    </item>
    <item>
      <title>Re: Timeout error when flashing IMX8Mplus using UUU</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Timeout-error-when-flashing-IMX8Mplus-using-UUU/m-p/1497955#M193204</link>
      <description>&lt;P&gt;Here maybe caused by the usb, for the usb USB 2.0 design you need to see the&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-i-MX8MQ-USB2-0-Design-Without-USB-TYPE-C/ta-p/1129527" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-i-MX8MQ-USB2-0-Design-Without-USB-TYPE-C/ta-p/1129527&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;To see if this section will be OK.&lt;/P&gt;
&lt;P&gt;For the DDR you also need to configure proper parameters.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jul 2022 09:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Timeout-error-when-flashing-IMX8Mplus-using-UUU/m-p/1497955#M193204</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2022-07-29T09:48:00Z</dc:date>
    </item>
  </channel>
</rss>