<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX280 power on reset threshold voltage</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX280-power-on-reset-threshold-voltage/m-p/1490945#M192656</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I have a question with IMX280DVM4B power on reset voltage.&lt;/P&gt;&lt;P&gt;Application note "IMX28CEC" said&amp;nbsp; "Because the i.MX28 is a PMU and an SoC, power-on reset is generated internally and there is no timing&amp;nbsp;requirement on external pins."&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it didn't mention the specific power on reset threshold voltage.&lt;/P&gt;&lt;P&gt;Now we plan to add external reset circuit to control "RESETN" pin by monitoring VDD5V power source. so I would like to know the exact&amp;nbsp;power on reset threshold value for&amp;nbsp;i.MX280 internal design. Probably we are able to refer to the threshold voltage.&lt;/P&gt;</description>
    <pubDate>Mon, 18 Jul 2022 09:05:18 GMT</pubDate>
    <dc:creator>Cookie456</dc:creator>
    <dc:date>2022-07-18T09:05:18Z</dc:date>
    <item>
      <title>IMX280 power on reset threshold voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX280-power-on-reset-threshold-voltage/m-p/1490945#M192656</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I have a question with IMX280DVM4B power on reset voltage.&lt;/P&gt;&lt;P&gt;Application note "IMX28CEC" said&amp;nbsp; "Because the i.MX28 is a PMU and an SoC, power-on reset is generated internally and there is no timing&amp;nbsp;requirement on external pins."&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it didn't mention the specific power on reset threshold voltage.&lt;/P&gt;&lt;P&gt;Now we plan to add external reset circuit to control "RESETN" pin by monitoring VDD5V power source. so I would like to know the exact&amp;nbsp;power on reset threshold value for&amp;nbsp;i.MX280 internal design. Probably we are able to refer to the threshold voltage.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 09:05:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX280-power-on-reset-threshold-voltage/m-p/1490945#M192656</guid>
      <dc:creator>Cookie456</dc:creator>
      <dc:date>2022-07-18T09:05:18Z</dc:date>
    </item>
    <item>
      <title>Re: IMX280 power on reset threshold voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX280-power-on-reset-threshold-voltage/m-p/1497943#M193201</link>
      <description>&lt;P&gt;Recommend you to use our reference design.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jul 2022 09:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX280-power-on-reset-threshold-voltage/m-p/1497943#M193201</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2022-07-29T09:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX280 power on reset threshold voltage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX280-power-on-reset-threshold-voltage/m-p/1498407#M193235</link>
      <description>&lt;P&gt;There is a manual reset circuit in our current design. It is similar with NXP reference design. but it is not able to solve the problem we meet now. when VDD_5V falls below 4.75V due to power interuption, power supply recovers before VDD_5V falls to zero,but the system can't restart automatically. so we plan to add an external reset circuit by monitoring VDD_5V in order to realize system restart automatically.&lt;BR /&gt;So could you please check power on reset threshold voltage internally? or do you hanve any other recommendations to solve this problem?&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 01:28:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX280-power-on-reset-threshold-voltage/m-p/1498407#M193235</guid>
      <dc:creator>Cookie456</dc:creator>
      <dc:date>2022-08-01T01:28:55Z</dc:date>
    </item>
  </channel>
</rss>