<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: eMMC Host controller in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Host-controller/m-p/1490118#M192582</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did not find any info from the reference design or user's guide that mention if the configuration of the eMMC controller in the EVK board is set to push-pull or not. Could you advise where I can get the info?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 15 Jul 2022 07:04:01 GMT</pubDate>
    <dc:creator>Danz1</dc:creator>
    <dc:date>2022-07-15T07:04:01Z</dc:date>
    <item>
      <title>eMMC Host controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Host-controller/m-p/1480133#M191923</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Does the eMMC Host Controller in iMX8M operates in push-pull mode?&lt;/P&gt;&lt;P&gt;Is the value of the push-pull resistors according to the pull-up/down resistors shows in Table 27? Thanks.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GPIO_DC_parameters.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/184648iE259A0E67E5F06B0/image-size/large?v=v2&amp;amp;px=999" role="button" title="GPIO_DC_parameters.jpg" alt="GPIO_DC_parameters.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;GPIO_DC_parameters.jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 26 Jun 2022 22:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-Host-controller/m-p/1480133#M191923</guid>
      <dc:creator>Danz1</dc:creator>
      <dc:date>2022-06-26T22:15:52Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC Host controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Host-controller/m-p/1489315#M192524</link>
      <description>&lt;P&gt;Please refer to the reference design.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 08:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-Host-controller/m-p/1489315#M192524</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2022-07-14T08:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC Host controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Host-controller/m-p/1490118#M192582</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did not find any info from the reference design or user's guide that mention if the configuration of the eMMC controller in the EVK board is set to push-pull or not. Could you advise where I can get the info?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jul 2022 07:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-Host-controller/m-p/1490118#M192582</guid>
      <dc:creator>Danz1</dc:creator>
      <dc:date>2022-07-15T07:04:01Z</dc:date>
    </item>
  </channel>
</rss>