<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Root Filesystem Encryption/Decryption with CAAM on an i.MX8M-Mini</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1489640#M192560</link>
    <description>&lt;P&gt;people typically use an initramfs for this. you can also use u-boot but I don't think there is caam support in u-boot.&lt;/P&gt;</description>
    <pubDate>Thu, 14 Jul 2022 17:21:09 GMT</pubDate>
    <dc:creator>richc128</dc:creator>
    <dc:date>2022-07-14T17:21:09Z</dc:date>
    <item>
      <title>Root Filesystem Encryption/Decryption with CAAM on an i.MX8M-Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1484070#M192159</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I was wondering if you could direct on how to encrypt, and decrypt, a Linux root filesystem using CAAM on an &lt;SPAN&gt;i.MX8M-Mini&lt;/SPAN&gt;?&lt;/P&gt;&lt;P&gt;I've read AN12714 "i.MX Encrypted Storage Using CAAM Secure Keys" but that only shows me how to use CAAM to perform encryption on a flat-file in an already booted OS. What I am looking for is how to decrypt the root filesystem during boot using CAAM.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;&lt;SPAN&gt;Bob&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jul 2022 12:32:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1484070#M192159</guid>
      <dc:creator>bobjenkins</dc:creator>
      <dc:date>2022-07-04T12:32:13Z</dc:date>
    </item>
    <item>
      <title>Re: Root Filesystem Encryption/Decryption with CAAM on an i.MX8M-Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1486412#M192311</link>
      <description>&lt;P&gt;you can just replace the looper with the drive / partition device. But, that being said, I've had consistent problems with re-mounting&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/AN12714-can-t-re-mount-encrypted-drive/m-p/1485545#M192249" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/AN12714-can-t-re-mount-encrypted-drive/m-p/1485545#M192249&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 20:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1486412#M192311</guid>
      <dc:creator>richc128</dc:creator>
      <dc:date>2022-07-07T20:52:48Z</dc:date>
    </item>
    <item>
      <title>Re: Root Filesystem Encryption/Decryption with CAAM on an i.MX8M-Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1488299#M192446</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, thanks for the tip! I am able to do "disk image" file or full, non-root, partition encryption as per the example in AN12714. However, this is from a non-encrypted root filesystem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I am unsure about is if I encrypt the entire root (/) partition/filesystem with CAAM, how would I be able to get the early stage of the kernel to decrypt that root filesystem during boot, using the Black Blob/Black Key/imported session key from CAAM?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The kernel would need to do this decryption early in the boot process, as with the root (/) filesystem being encrypted at this point, the kernel modules (/lib/modules/...), config files (/etc/...), executables (/bin/...), etc. would be unavailable to the kernel and OS later in boot, if it isn't decrypted with CAAM early&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any advice would be greatly appreciated!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 19:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1488299#M192446</guid>
      <dc:creator>bobjenkins</dc:creator>
      <dc:date>2022-07-12T19:18:16Z</dc:date>
    </item>
    <item>
      <title>Re: Root Filesystem Encryption/Decryption with CAAM on an i.MX8M-Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1489640#M192560</link>
      <description>&lt;P&gt;people typically use an initramfs for this. you can also use u-boot but I don't think there is caam support in u-boot.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 17:21:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Root-Filesystem-Encryption-Decryption-with-CAAM-on-an-i-MX8M/m-p/1489640#M192560</guid>
      <dc:creator>richc128</dc:creator>
      <dc:date>2022-07-14T17:21:09Z</dc:date>
    </item>
  </channel>
</rss>