<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6Q EMMC Flash is not working Android 9</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-EMMC-Flash-is-not-working-Android-9/m-p/1488165#M192435</link>
    <description>&lt;P&gt;Hello laulavanya,&lt;/P&gt;
&lt;P&gt;The Android 9 BSP doesn't work with i.MX6Q, it use the 64 bit only for compilation and deployment, you have to use the Android 8, or go to the community bsp.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 12 Jul 2022 13:32:55 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2022-07-12T13:32:55Z</dc:date>
    <item>
      <title>IMX6Q EMMC Flash is not working Android 9</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-EMMC-Flash-is-not-working-Android-9/m-p/1486886#M192337</link>
      <description>&lt;P&gt;Hi NXP,&lt;BR /&gt;&lt;BR /&gt;Sdcard flash is working for android 9&lt;BR /&gt;&lt;BR /&gt;Emmc :&lt;BR /&gt;Able to flash the binaries using uuu tool but unable to boot.&lt;BR /&gt;&lt;BR /&gt;Facing below issue&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Can somebody identify quickly?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... MMC: no card present&lt;BR /&gt;*** Warning - No block device, using default environment&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;BR /&gt;No panel detected: default to ConsoleUI-XGA&lt;BR /&gt;Display: ConsoleUI-XGA (1280x800)&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;MMC: no card present&lt;BR /&gt;MMC card init failed!&lt;BR /&gt;MMC: no card present&lt;BR /&gt;** Block device MMC 1 not supported&lt;BR /&gt;Net: No ethernet found.&lt;BR /&gt;MMC: no card present&lt;BR /&gt;Block device mmc 1 not supported&lt;BR /&gt;bcb_rw_block, get_block_size return 0&lt;BR /&gt;read_bootctl, bcb_rw_block read failed&lt;BR /&gt;read command failed&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;cannot get the partion info for fbmisc&lt;BR /&gt;fastboot_get_lock_stat: error in get mmc part&lt;BR /&gt;MMC: no card present&lt;BR /&gt;fsl_read_from_partition_multi: mmc device not found&lt;BR /&gt;MMC: no card present&lt;BR /&gt;fsl_read_from_partition_multi: mmc device not found&lt;BR /&gt;avb_slot_verify.c:603: ERROR: boot: Error loading footer.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jul 2022 14:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-EMMC-Flash-is-not-working-Android-9/m-p/1486886#M192337</guid>
      <dc:creator>laulavanya</dc:creator>
      <dc:date>2022-07-08T14:33:17Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q EMMC Flash is not working Android 9</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-EMMC-Flash-is-not-working-Android-9/m-p/1488165#M192435</link>
      <description>&lt;P&gt;Hello laulavanya,&lt;/P&gt;
&lt;P&gt;The Android 9 BSP doesn't work with i.MX6Q, it use the 64 bit only for compilation and deployment, you have to use the Android 8, or go to the community bsp.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 13:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-EMMC-Flash-is-not-working-Android-9/m-p/1488165#M192435</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-07-12T13:32:55Z</dc:date>
    </item>
  </channel>
</rss>