<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Linux I2C custom message frame sending in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-I2C-custom-message-frame-sending/m-p/1487041#M192346</link>
    <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Is it possible to send out a custom message frame on I2C dev from Linux? I am using an i.MX7D board and i would like to use "/dev/i2c-0" device like a simple "serial tty" to "write(fd, bytes, count)". My goal is to send out a single byte for example 0xAB on I2C without any specific slave address and without automatic stop/start bit inserting in my frame.&lt;/P&gt;&lt;P&gt;So i like to make my full custom I2C frame then send it out from Linux. Is it possible, is there any user-space programing techniques in C/C++, Python or any API for it in Linux?&lt;/P&gt;</description>
    <pubDate>Sat, 09 Jul 2022 12:25:37 GMT</pubDate>
    <dc:creator>Livius</dc:creator>
    <dc:date>2022-07-09T12:25:37Z</dc:date>
    <item>
      <title>Linux I2C custom message frame sending</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-I2C-custom-message-frame-sending/m-p/1487041#M192346</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Is it possible to send out a custom message frame on I2C dev from Linux? I am using an i.MX7D board and i would like to use "/dev/i2c-0" device like a simple "serial tty" to "write(fd, bytes, count)". My goal is to send out a single byte for example 0xAB on I2C without any specific slave address and without automatic stop/start bit inserting in my frame.&lt;/P&gt;&lt;P&gt;So i like to make my full custom I2C frame then send it out from Linux. Is it possible, is there any user-space programing techniques in C/C++, Python or any API for it in Linux?&lt;/P&gt;</description>
      <pubDate>Sat, 09 Jul 2022 12:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-I2C-custom-message-frame-sending/m-p/1487041#M192346</guid>
      <dc:creator>Livius</dc:creator>
      <dc:date>2022-07-09T12:25:37Z</dc:date>
    </item>
  </channel>
</rss>