<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRead bootrom log imx8mq</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Read-bootrom-log-imx8mq/m-p/1486705#M192326</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to check bootrom log events on imx8mq processor. Following AN12853 I understand that imx8mq have:&lt;BR /&gt;ROM event ID definition version 2&lt;/P&gt;&lt;P&gt;and&amp;nbsp;ROM event ID format version 1 so it means bits 24:31 are valid.&lt;/P&gt;&lt;P&gt;I found base address of OCRAM in ATF and it should be 0x900000. Buffer should start at 0x9E0.&lt;/P&gt;&lt;P&gt;SO when booted board and in u-boot I run:&lt;/P&gt;&lt;P&gt;md.l 0x9009E0 1 I got:&lt;/P&gt;&lt;P&gt;u-boot=&amp;gt; md.l 0x9009e0 1&lt;BR /&gt;009009e0: 23d1786f ox.#&lt;/P&gt;&lt;P&gt;so from above log should be 0x23d1 (as only 16 bits are valid). But it doesn't make sense to me as in begnning of appnote is written that:&lt;/P&gt;&lt;P&gt;ROM even entry have bites 0-4 ROM event ID which is only 4 bits and not byte. Maybe I overlooked something? Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 08 Jul 2022 08:19:37 GMT</pubDate>
    <dc:creator>marekb</dc:creator>
    <dc:date>2022-07-08T08:19:37Z</dc:date>
    <item>
      <title>Read bootrom log imx8mq</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Read-bootrom-log-imx8mq/m-p/1486705#M192326</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to check bootrom log events on imx8mq processor. Following AN12853 I understand that imx8mq have:&lt;BR /&gt;ROM event ID definition version 2&lt;/P&gt;&lt;P&gt;and&amp;nbsp;ROM event ID format version 1 so it means bits 24:31 are valid.&lt;/P&gt;&lt;P&gt;I found base address of OCRAM in ATF and it should be 0x900000. Buffer should start at 0x9E0.&lt;/P&gt;&lt;P&gt;SO when booted board and in u-boot I run:&lt;/P&gt;&lt;P&gt;md.l 0x9009E0 1 I got:&lt;/P&gt;&lt;P&gt;u-boot=&amp;gt; md.l 0x9009e0 1&lt;BR /&gt;009009e0: 23d1786f ox.#&lt;/P&gt;&lt;P&gt;so from above log should be 0x23d1 (as only 16 bits are valid). But it doesn't make sense to me as in begnning of appnote is written that:&lt;/P&gt;&lt;P&gt;ROM even entry have bites 0-4 ROM event ID which is only 4 bits and not byte. Maybe I overlooked something? Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jul 2022 08:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Read-bootrom-log-imx8mq/m-p/1486705#M192326</guid>
      <dc:creator>marekb</dc:creator>
      <dc:date>2022-07-08T08:19:37Z</dc:date>
    </item>
  </channel>
</rss>