<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFavorite Embedded Timing and Profiling Tool?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Favorite-Embedded-Timing-and-Profiling-Tool/m-p/1485724#M192257</link>
    <description>&lt;P&gt;Hi. I dev on an i.MX 1060.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-mcus/i-mx-rt1060-crossover-mcu-with-arm-cortex-m7-core:i.MX-RT1060" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-mcus/i-mx-rt1060-crossover-mcu-with-arm-cortex-m7-core:i.MX-RT1060&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Recently I had an issue wherein I was time constrained and didn't know which part of my code was taking the longest. I had control of GPIO anyway inside the program, so I set/unset the GPIO and measured timings with a Saleae Logic Analyzer. (Another piece of debug hardware which has saved my but more times than I can count)&lt;/P&gt;&lt;P&gt;My question is. This is the way I've done this kind of tight sub millisecond debugging in the past, however, I'd like to find an on-board utility that does this and I'd like to up my game.&lt;/P&gt;&lt;P&gt;Are there any tools that can code profile for me with sub ms accuracy? Commericial or otherwise. Does anything by Segger do this?&lt;/P&gt;&lt;P&gt;I'd also be willing to learn about fast ARM timers I can use for very accurate timing.&lt;/P&gt;&lt;P&gt;I've also resorted to RTOS timers for timing, but it just feels too clumsy and slow. I need something better.&lt;/P&gt;&lt;P&gt;It'd be great if this tools could be taken across the ARM ecosystem.&lt;/P&gt;&lt;P&gt;Thanks! so much.&lt;/P&gt;</description>
    <pubDate>Wed, 06 Jul 2022 21:08:57 GMT</pubDate>
    <dc:creator>engi_2068</dc:creator>
    <dc:date>2022-07-06T21:08:57Z</dc:date>
    <item>
      <title>Favorite Embedded Timing and Profiling Tool?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Favorite-Embedded-Timing-and-Profiling-Tool/m-p/1485724#M192257</link>
      <description>&lt;P&gt;Hi. I dev on an i.MX 1060.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-mcus/i-mx-rt1060-crossover-mcu-with-arm-cortex-m7-core:i.MX-RT1060" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-mcus/i-mx-rt1060-crossover-mcu-with-arm-cortex-m7-core:i.MX-RT1060&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Recently I had an issue wherein I was time constrained and didn't know which part of my code was taking the longest. I had control of GPIO anyway inside the program, so I set/unset the GPIO and measured timings with a Saleae Logic Analyzer. (Another piece of debug hardware which has saved my but more times than I can count)&lt;/P&gt;&lt;P&gt;My question is. This is the way I've done this kind of tight sub millisecond debugging in the past, however, I'd like to find an on-board utility that does this and I'd like to up my game.&lt;/P&gt;&lt;P&gt;Are there any tools that can code profile for me with sub ms accuracy? Commericial or otherwise. Does anything by Segger do this?&lt;/P&gt;&lt;P&gt;I'd also be willing to learn about fast ARM timers I can use for very accurate timing.&lt;/P&gt;&lt;P&gt;I've also resorted to RTOS timers for timing, but it just feels too clumsy and slow. I need something better.&lt;/P&gt;&lt;P&gt;It'd be great if this tools could be taken across the ARM ecosystem.&lt;/P&gt;&lt;P&gt;Thanks! so much.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 21:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Favorite-Embedded-Timing-and-Profiling-Tool/m-p/1485724#M192257</guid>
      <dc:creator>engi_2068</dc:creator>
      <dc:date>2022-07-06T21:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: Favorite Embedded Timing and Profiling Tool?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Favorite-Embedded-Timing-and-Profiling-Tool/m-p/1485863#M192268</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/113802"&gt;@engi_2068&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;MCUXpresso IDE has SWO profile function. I think this is fit for your case. Please see chapter 2 in MCUXpresso_IDE_SWO_Trace.pdf.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 03:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Favorite-Embedded-Timing-and-Profiling-Tool/m-p/1485863#M192268</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-07-07T03:17:20Z</dc:date>
    </item>
  </channel>
</rss>