<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Load application from QSPI to RAM - imx7ulp</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Load-application-from-QSPI-to-RAM-imx7ulp/m-p/1485480#M192242</link>
    <description>&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 06 Jul 2022 14:07:36 GMT</pubDate>
    <dc:creator>klaas</dc:creator>
    <dc:date>2022-07-06T14:07:36Z</dc:date>
    <item>
      <title>Load application from QSPI to RAM - imx7ulp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Load-application-from-QSPI-to-RAM-imx7ulp/m-p/1483342#M192107</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm trying to write a costum bootloader for the CM4 on a imx7ulp using IAR EWARM.&lt;/P&gt;&lt;P&gt;My goal is to manually copy the application from QSPI and then execute it.&lt;/P&gt;&lt;P&gt;To me this seems to be a common use-case but I can't find any examples helping me. Mainly I'm not sure which parts of the image residing in the QSPI I need to copy in which locations of the RAM.&lt;/P&gt;&lt;P&gt;Any help or links to examples are welcome!&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Klaas&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jul 2022 09:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Load-application-from-QSPI-to-RAM-imx7ulp/m-p/1483342#M192107</guid>
      <dc:creator>klaas</dc:creator>
      <dc:date>2022-07-01T09:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: Load application from QSPI to RAM - imx7ulp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Load-application-from-QSPI-to-RAM-imx7ulp/m-p/1485480#M192242</link>
      <description>&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 14:07:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Load-application-from-QSPI-to-RAM-imx7ulp/m-p/1485480#M192242</guid>
      <dc:creator>klaas</dc:creator>
      <dc:date>2022-07-06T14:07:36Z</dc:date>
    </item>
  </channel>
</rss>