<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is it possible to enable LVDS over DT overlay? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-enable-LVDS-over-DT-overlay/m-p/1483842#M192144</link>
    <description>&lt;P&gt;I am trying to enable LVDS over a DeviceTree overlay.&lt;BR /&gt;Why?&lt;BR /&gt;I have a baseboard with a i.MX8MP SOM. This baseboard can have more or less features depending on the assambling. Furthermore I want to connect different LVDS panels (7"/10") to this board.&lt;BR /&gt;The feature set of this board should automatic set by loading different device-tree overlays. Every feature get its own overlay. For example:&lt;BR /&gt;Sound -&amp;gt; sound.dtbo&lt;BR /&gt;Temprature -&amp;gt; temp.dtbo&lt;BR /&gt;Ethernet -&amp;gt; eth.dtbo&lt;BR /&gt;All this overlays should load by a systemd service as early as possible.&lt;BR /&gt;All features work fine but not the LVDS. I can't get it work.&lt;BR /&gt;I need to set the panel driver and the backlight settings in the overlay.&lt;BR /&gt;Is there a way to define a dummy panel and overwrite it with the DT overlay? I tried to enable all (LCD-Controller, LVDS, ldb, ldb-pyh) in my overlay but the kernel does not do a probe after loading the overlay.&lt;/P&gt;</description>
    <pubDate>Mon, 04 Jul 2022 06:28:34 GMT</pubDate>
    <dc:creator>MicMoba</dc:creator>
    <dc:date>2022-07-04T06:28:34Z</dc:date>
    <item>
      <title>Is it possible to enable LVDS over DT overlay?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-enable-LVDS-over-DT-overlay/m-p/1483842#M192144</link>
      <description>&lt;P&gt;I am trying to enable LVDS over a DeviceTree overlay.&lt;BR /&gt;Why?&lt;BR /&gt;I have a baseboard with a i.MX8MP SOM. This baseboard can have more or less features depending on the assambling. Furthermore I want to connect different LVDS panels (7"/10") to this board.&lt;BR /&gt;The feature set of this board should automatic set by loading different device-tree overlays. Every feature get its own overlay. For example:&lt;BR /&gt;Sound -&amp;gt; sound.dtbo&lt;BR /&gt;Temprature -&amp;gt; temp.dtbo&lt;BR /&gt;Ethernet -&amp;gt; eth.dtbo&lt;BR /&gt;All this overlays should load by a systemd service as early as possible.&lt;BR /&gt;All features work fine but not the LVDS. I can't get it work.&lt;BR /&gt;I need to set the panel driver and the backlight settings in the overlay.&lt;BR /&gt;Is there a way to define a dummy panel and overwrite it with the DT overlay? I tried to enable all (LCD-Controller, LVDS, ldb, ldb-pyh) in my overlay but the kernel does not do a probe after loading the overlay.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jul 2022 06:28:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-enable-LVDS-over-DT-overlay/m-p/1483842#M192144</guid>
      <dc:creator>MicMoba</dc:creator>
      <dc:date>2022-07-04T06:28:34Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to enable LVDS over DT overlay?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-enable-LVDS-over-DT-overlay/m-p/1487187#M192363</link>
      <description>&lt;P&gt;It seems that it is not possible. I solved this issue by applying the DT overlay for my LVDS during the uboot. Afterwards I apply all other DT overlays with a systemd service.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jul 2022 04:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-enable-LVDS-over-DT-overlay/m-p/1487187#M192363</guid>
      <dc:creator>MicMoba</dc:creator>
      <dc:date>2022-07-11T04:52:50Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to enable LVDS over DT overlay?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-enable-LVDS-over-DT-overlay/m-p/1487204#M192365</link>
      <description>&lt;P&gt;Facing same issue here. Help is appreciated.&amp;nbsp;&amp;nbsp;&lt;A href="https://www.myatriumhealth.us/" target="_self"&gt;&lt;FONT color="#FFFFFF"&gt;MyAtriumHealth Login&lt;/FONT&gt;&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jul 2022 05:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-enable-LVDS-over-DT-overlay/m-p/1487204#M192365</guid>
      <dc:creator>smitgh20562</dc:creator>
      <dc:date>2022-07-11T05:38:15Z</dc:date>
    </item>
  </channel>
</rss>