<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRT1064 how to use PWMX module</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1064-how-to-use-PWMX-module/m-p/1483655#M192130</link>
    <description>&lt;P&gt;Because of some requirements of the project, I use the PWMX module of flexPWM to control GPIO_AD_B0_02 to output PWM. The reference manual says that no mapping is required, and PWM can be output directly, but I found that I have no way to start. The examples in the manual are not as detailed as other modules, and my strength is limited. , please help me find out what to do. thanks&lt;/P&gt;</description>
    <pubDate>Sun, 03 Jul 2022 11:00:26 GMT</pubDate>
    <dc:creator>Alexander-cloud</dc:creator>
    <dc:date>2022-07-03T11:00:26Z</dc:date>
    <item>
      <title>RT1064 how to use PWMX module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1064-how-to-use-PWMX-module/m-p/1483655#M192130</link>
      <description>&lt;P&gt;Because of some requirements of the project, I use the PWMX module of flexPWM to control GPIO_AD_B0_02 to output PWM. The reference manual says that no mapping is required, and PWM can be output directly, but I found that I have no way to start. The examples in the manual are not as detailed as other modules, and my strength is limited. , please help me find out what to do. thanks&lt;/P&gt;</description>
      <pubDate>Sun, 03 Jul 2022 11:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1064-how-to-use-PWMX-module/m-p/1483655#M192130</guid>
      <dc:creator>Alexander-cloud</dc:creator>
      <dc:date>2022-07-03T11:00:26Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 how to use PWMX module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1064-how-to-use-PWMX-module/m-p/1487594#M192397</link>
      <description>&lt;P&gt;Hi Alexander,&lt;/P&gt;
&lt;P&gt;Thank you so much for using our community.&lt;/P&gt;
&lt;P&gt;I suggest you, refer to the evkmimxrt1064_pwm SDK example and with the help of Config Tools you can configure that pin you want, you would only have to make slight configuration modifications.&lt;/P&gt;
&lt;P&gt;I hope this will help you. Please let me know if you have more questions about it.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jul 2022 17:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1064-how-to-use-PWMX-module/m-p/1487594#M192397</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-07-11T17:21:02Z</dc:date>
    </item>
  </channel>
</rss>