<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Recompiled Image Causing Reboot Loop in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Recompiled-Image-Causing-Reboot-Loop/m-p/1483604#M192120</link>
    <description>&lt;P&gt;Using an &lt;SPAN class=""&gt;MCIMX6ULL-EVK&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;I have been trying to get my build system working with the end goal adding spidev to the linux userspace.&lt;/P&gt;&lt;P&gt;With the first step of simply compiling Linux on my system and verify that the board can boot correctly.&lt;/P&gt;&lt;P&gt;However, the kernels and SD card images my system is producing are not working. I don't know what the kernel is doing because it doesn't print to the terminal. It could be in an infinite loop for all I know.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Description of my process:&lt;/P&gt;&lt;P&gt;Using the provided SD card, pre-flashed with distribution 4.9.88_2.0.0, the board boots up correctly and I can log in over serial.&lt;/P&gt;&lt;P&gt;I have been approaching this problem from two directions:&lt;/P&gt;&lt;P&gt;1. Recompiling Linux with the appropriate&lt;FONT face="courier new,courier"&gt; imx_v6_v7_defconfig&lt;/FONT&gt;, and dropping the resulting &lt;FONT face="courier new,courier"&gt;zImage&lt;/FONT&gt; onto the SD card. Note that the Linux kernel is&lt;FONT face="courier new,courier"&gt; v5.15.31&lt;/FONT&gt;, and the corresponding SDK environment used to build Linux is &lt;FONT face="courier new,courier"&gt;5.15-kirkstone&lt;/FONT&gt;.&lt;/P&gt;&lt;P&gt;However, once I power on the system, U-boot reads and starts the new kernel. But that's the end of that since I it never prints any more output afterwards.&lt;/P&gt;&lt;P&gt;2. Recompiling the whole system using Yocto using:&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;bitbake core-image-minimal&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;And either dropping the resulting zImage onto the SD card, or writing the whole &lt;FONT face="courier new,courier"&gt;core-image-base-imx6ulevk.wic &lt;FONT face="arial,helvetica,sans-serif"&gt;to another SD card, in which case, the system performs an endless reboot loop. Producing this output:&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;CPU:   Commercial temperature grade (0C to 95C) at 42C
Reset cause: POR
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM:  512 MiB
Core:  63 devices, 18 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
        [0] lcdif@21c8000, video
In:    serial
Out:   serial
Err:   serial
data abort
pc : [&amp;lt;9eea1e2a&amp;gt;]          lr : [&amp;lt;9eec0a51&amp;gt;]
reloc pc : [&amp;lt;87823e2a&amp;gt;]    lr : [&amp;lt;87842a51&amp;gt;]
sp : 9de748a0  ip : 9de7488c     fp : 87800020
r10: 00000017  r9 : 9de7bec0     r8 : 00000100
r7 : 021bc400  r6 : 9eecd9e5     r5 : 00000000  r4 : 9de7e9d0
r3 : ffffffff  r2 : 02140000     r1 : 00006cc8  r0 : ffffffff
Flags: NzCv  IRQs off  FIQs off  Mode SVC_32 (T)
Code: 1e03 9300 da0e 6822 (6853) b125
Resetting CPU ...

resetting ...&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I drop the new Yocto zImage onto the SD card like I did for the linux kernel only compilation, It stops printing after U-boot jumps into the kernel just like in the first scenario I listed above.&lt;/P&gt;</description>
    <pubDate>Fri, 01 Jul 2022 23:56:41 GMT</pubDate>
    <dc:creator>robwasab</dc:creator>
    <dc:date>2022-07-01T23:56:41Z</dc:date>
    <item>
      <title>Recompiled Image Causing Reboot Loop</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recompiled-Image-Causing-Reboot-Loop/m-p/1483604#M192120</link>
      <description>&lt;P&gt;Using an &lt;SPAN class=""&gt;MCIMX6ULL-EVK&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;I have been trying to get my build system working with the end goal adding spidev to the linux userspace.&lt;/P&gt;&lt;P&gt;With the first step of simply compiling Linux on my system and verify that the board can boot correctly.&lt;/P&gt;&lt;P&gt;However, the kernels and SD card images my system is producing are not working. I don't know what the kernel is doing because it doesn't print to the terminal. It could be in an infinite loop for all I know.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Description of my process:&lt;/P&gt;&lt;P&gt;Using the provided SD card, pre-flashed with distribution 4.9.88_2.0.0, the board boots up correctly and I can log in over serial.&lt;/P&gt;&lt;P&gt;I have been approaching this problem from two directions:&lt;/P&gt;&lt;P&gt;1. Recompiling Linux with the appropriate&lt;FONT face="courier new,courier"&gt; imx_v6_v7_defconfig&lt;/FONT&gt;, and dropping the resulting &lt;FONT face="courier new,courier"&gt;zImage&lt;/FONT&gt; onto the SD card. Note that the Linux kernel is&lt;FONT face="courier new,courier"&gt; v5.15.31&lt;/FONT&gt;, and the corresponding SDK environment used to build Linux is &lt;FONT face="courier new,courier"&gt;5.15-kirkstone&lt;/FONT&gt;.&lt;/P&gt;&lt;P&gt;However, once I power on the system, U-boot reads and starts the new kernel. But that's the end of that since I it never prints any more output afterwards.&lt;/P&gt;&lt;P&gt;2. Recompiling the whole system using Yocto using:&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;bitbake core-image-minimal&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;And either dropping the resulting zImage onto the SD card, or writing the whole &lt;FONT face="courier new,courier"&gt;core-image-base-imx6ulevk.wic &lt;FONT face="arial,helvetica,sans-serif"&gt;to another SD card, in which case, the system performs an endless reboot loop. Producing this output:&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;CPU:   Commercial temperature grade (0C to 95C) at 42C
Reset cause: POR
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM:  512 MiB
Core:  63 devices, 18 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
        [0] lcdif@21c8000, video
In:    serial
Out:   serial
Err:   serial
data abort
pc : [&amp;lt;9eea1e2a&amp;gt;]          lr : [&amp;lt;9eec0a51&amp;gt;]
reloc pc : [&amp;lt;87823e2a&amp;gt;]    lr : [&amp;lt;87842a51&amp;gt;]
sp : 9de748a0  ip : 9de7488c     fp : 87800020
r10: 00000017  r9 : 9de7bec0     r8 : 00000100
r7 : 021bc400  r6 : 9eecd9e5     r5 : 00000000  r4 : 9de7e9d0
r3 : ffffffff  r2 : 02140000     r1 : 00006cc8  r0 : ffffffff
Flags: NzCv  IRQs off  FIQs off  Mode SVC_32 (T)
Code: 1e03 9300 da0e 6822 (6853) b125
Resetting CPU ...

resetting ...&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I drop the new Yocto zImage onto the SD card like I did for the linux kernel only compilation, It stops printing after U-boot jumps into the kernel just like in the first scenario I listed above.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jul 2022 23:56:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recompiled-Image-Causing-Reboot-Loop/m-p/1483604#M192120</guid>
      <dc:creator>robwasab</dc:creator>
      <dc:date>2022-07-01T23:56:41Z</dc:date>
    </item>
    <item>
      <title>Re: Recompiled Image Causing Reboot Loop</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recompiled-Image-Causing-Reboot-Loop/m-p/1684925#M208974</link>
      <description>&lt;P&gt;Hi!&lt;BR /&gt;I unfortunately face the exact same issue with the exact same hardware.&lt;/P&gt;&lt;P&gt;Did you figure out how to solve this issue?&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 13:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recompiled-Image-Causing-Reboot-Loop/m-p/1684925#M208974</guid>
      <dc:creator>bguende</dc:creator>
      <dc:date>2023-07-10T13:12:33Z</dc:date>
    </item>
  </channel>
</rss>