<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSecure Provisioning Tool error XIP encrypted (BEE OTPMK) authenticated and HAB disabled</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Provisioning-Tool-error-XIP-encrypted-BEE-OTPMK/m-p/1481902#M192020</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm following &lt;A href="https://www.nxp.com/design/training/secure-boot-on-the-i-mx-rt10xx-crossover-mcus:TIP-SECURE-BOOT-ON-THE-I.MX-RT10XX-CROSSOVER-MCUS" target="_self"&gt;this webinar&lt;/A&gt; to learn how to use the Secure Provisioning Tool with an i.MX RT1060 with different types of boot.&lt;/P&gt;&lt;P&gt;As I'm in the learning phase, I'm using the "Open, HAB disabled" life cycle option in the Secure Provisioning Tool (version 4.0.1)&lt;/P&gt;&lt;P&gt;But when I try and use the last boot type demo'd in the webinar which is XIP encrypted (BEE OTPMK) authenticated with the life cycle selected as Open, HAB disabled I get this error in the Log&amp;nbsp;&lt;/P&gt;&lt;P&gt;"It is not possible to create encrypted image with disabled security" (see attached image of error)&lt;/P&gt;&lt;P&gt;Can someone help me understand why this is?&amp;nbsp;&lt;/P&gt;&lt;P&gt;If it helps I'm using and MIMXRT1060-EVKB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 29 Jun 2022 14:49:25 GMT</pubDate>
    <dc:creator>mkarandikar</dc:creator>
    <dc:date>2022-06-29T14:49:25Z</dc:date>
    <item>
      <title>Secure Provisioning Tool error XIP encrypted (BEE OTPMK) authenticated and HAB disabled</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Provisioning-Tool-error-XIP-encrypted-BEE-OTPMK/m-p/1481902#M192020</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm following &lt;A href="https://www.nxp.com/design/training/secure-boot-on-the-i-mx-rt10xx-crossover-mcus:TIP-SECURE-BOOT-ON-THE-I.MX-RT10XX-CROSSOVER-MCUS" target="_self"&gt;this webinar&lt;/A&gt; to learn how to use the Secure Provisioning Tool with an i.MX RT1060 with different types of boot.&lt;/P&gt;&lt;P&gt;As I'm in the learning phase, I'm using the "Open, HAB disabled" life cycle option in the Secure Provisioning Tool (version 4.0.1)&lt;/P&gt;&lt;P&gt;But when I try and use the last boot type demo'd in the webinar which is XIP encrypted (BEE OTPMK) authenticated with the life cycle selected as Open, HAB disabled I get this error in the Log&amp;nbsp;&lt;/P&gt;&lt;P&gt;"It is not possible to create encrypted image with disabled security" (see attached image of error)&lt;/P&gt;&lt;P&gt;Can someone help me understand why this is?&amp;nbsp;&lt;/P&gt;&lt;P&gt;If it helps I'm using and MIMXRT1060-EVKB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jun 2022 14:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Provisioning-Tool-error-XIP-encrypted-BEE-OTPMK/m-p/1481902#M192020</guid>
      <dc:creator>mkarandikar</dc:creator>
      <dc:date>2022-06-29T14:49:25Z</dc:date>
    </item>
  </channel>
</rss>