<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: QSPI for IMX8M Plus</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-for-IMX8M-Plus/m-p/1481380#M191992</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If you mean that if it is possible that the binary file runs at QSPI/XIP, then yes it is possible, please refer to the getting started with MCUXpresso SDK for EVK-MIMX8MP.&lt;BR /&gt;&lt;BR /&gt;If you mean that M7 has access to the QSPI, then no, usually this peripheral is assigned to the Cortex-A, so we do not provide a driver for cortex-M.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Tue, 28 Jun 2022 20:39:00 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-06-28T20:39:00Z</dc:date>
    <item>
      <title>QSPI for IMX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-for-IMX8M-Plus/m-p/1481294#M191984</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could we use the QSPI for IMX8M Plus M7 ?&lt;/P&gt;&lt;P&gt;If it work, where can i find the driver ?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Wayne.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 15:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-for-IMX8M-Plus/m-p/1481294#M191984</guid>
      <dc:creator>waynechung2</dc:creator>
      <dc:date>2022-06-28T15:19:16Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI for IMX8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSPI-for-IMX8M-Plus/m-p/1481380#M191992</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If you mean that if it is possible that the binary file runs at QSPI/XIP, then yes it is possible, please refer to the getting started with MCUXpresso SDK for EVK-MIMX8MP.&lt;BR /&gt;&lt;BR /&gt;If you mean that M7 has access to the QSPI, then no, usually this peripheral is assigned to the Cortex-A, so we do not provide a driver for cortex-M.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 20:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSPI-for-IMX8M-Plus/m-p/1481380#M191992</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-06-28T20:39:00Z</dc:date>
    </item>
  </channel>
</rss>