<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1061 debugging issue (JLink) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1481264#M191982</link>
    <description>&lt;P&gt;I have been trying to get the NXP-MCUBoot utility to work but it refuses to connect over lpuart1. What test can it perform? I cant find anything about flash testing in the description of the tool.&lt;BR /&gt;&lt;BR /&gt;Yes, we see the same issues when debugging the the sdk examples.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;/Björn&lt;/P&gt;</description>
    <pubDate>Tue, 28 Jun 2022 14:20:07 GMT</pubDate>
    <dc:creator>bjorns</dc:creator>
    <dc:date>2022-06-28T14:20:07Z</dc:date>
    <item>
      <title>RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1475186#M191554</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are developing an application for NXP RT1061 (custom board) and are experiencing some issues when it comes to debugging.&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCU: MIMXRT1061CVL5B&lt;BR /&gt;Flash: IS25LP032D&lt;BR /&gt;Debuger: JLink Plus&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1. The JLink server seems to have problems halting the mcu after reset, when running and debugging from flash, hinting that we have faulty flash settings. (Flash configuration is appended at the end.)&lt;/P&gt;&lt;P&gt;This causes for example breakpoints in the beginning of main not to trigger. And possibly also other issues as described below.&lt;/P&gt;&lt;P&gt;Log from JLinkServer:&lt;BR /&gt;&lt;EM&gt;Received monitor command: reset&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ResetTarget() start&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Core did not halt on flash image verification. Assuming faulty flash settings.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Halting target manually.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ResetTarget() end&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;What causes this, do we have the wrong flash configuration?&lt;/P&gt;&lt;P&gt;2. We have no problem booting from the flash. However once a program is present in the flash the Jlink&amp;nbsp; Debugger is unable to reprogram the flash. Could be related to issue 1 since if we insert a delay in the beginning of main it works. We have some units which we at the moment are unable to recover because of this.&lt;BR /&gt;&lt;BR /&gt;We suspect that configuring the MPU or something similar to this prevent JLink from uploading its "Ram code" but we have not been able to confirm this. We have however tried to disable the MPU using JLink commander but have not been successful. The FlexRam module has default configuration (128k DTC, 128K ITC, 256K OC).&lt;/P&gt;&lt;P&gt;JLink Commander Log:&lt;BR /&gt;J-Link&amp;gt;exec EnableEraseAllFlashBanks&lt;BR /&gt;J-Link&amp;gt;erase&lt;BR /&gt;Without any given address range, Erase Chip will be executed&lt;BR /&gt;Erasing device...&lt;BR /&gt;****** Error: Failed to prepare RAMCode using RAM&lt;BR /&gt;Error while determining flash info (Bank @ 0x60000000)&lt;BR /&gt;ERROR: Erase returned with error code -1.&lt;/P&gt;&lt;P&gt;3. Starting a debug session takes a long time.&lt;/P&gt;&lt;P&gt;The time from when the program has been written to flash/ram and the triggering of the first breakpoint in main is long sometimes more than a minute. This could for some reason be a related to the application size since we do not experience this issue when running nxp's example applications. Our application is around 400k. This happens both if we execute from ram and flash.&lt;/P&gt;&lt;P&gt;We are using McuXpresso.&lt;/P&gt;&lt;P&gt;What could be causing this? Anything we can do to improve the debugging experience.&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;/Björn&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Flash config:&lt;/P&gt;&lt;P&gt;const flexspi_nor_config_t qspiflash_config = {&lt;BR /&gt;.memConfig =&lt;BR /&gt;{&lt;BR /&gt;.tag = FLEXSPI_CFG_BLK_TAG,&lt;BR /&gt;.version = FLEXSPI_CFG_BLK_VERSION,&lt;BR /&gt;.readSampleClksrc=kFlexSPIReadSampleClk_LoopbackFromDqsPad,&lt;BR /&gt;.csHoldTime = 3u,&lt;BR /&gt;.csSetupTime = 3u,&lt;BR /&gt;.sflashPadType = kSerialFlash_4Pads,&lt;BR /&gt;.serialClkFreq = kFlexSpiSerialClk_100MHz,&lt;BR /&gt;.sflashA1Size = 4u * 1024u * 1024u,&lt;BR /&gt;.lookupTable =&lt;BR /&gt;{&lt;BR /&gt;// 0 Read LUTs&lt;BR /&gt;FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),&lt;BR /&gt;FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),&lt;BR /&gt;0,0,&lt;/P&gt;&lt;P&gt;// 1 Read Status&lt;BR /&gt;FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x81, READ_SDR, FLEXSPI_1PAD, 0x04),&lt;BR /&gt;0,0,0,&lt;/P&gt;&lt;P&gt;// 2 Reserved&lt;BR /&gt;0,0,0,0,&lt;/P&gt;&lt;P&gt;// 3 Write Enable&lt;BR /&gt;FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP, FLEXSPI_1PAD, 0),&lt;BR /&gt;0,0,0,&lt;/P&gt;&lt;P&gt;// 4 Reserved&lt;BR /&gt;0,0,0,0,&lt;/P&gt;&lt;P&gt;// 5 Erase Sector&lt;BR /&gt;FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xD7, RADDR_SDR, FLEXSPI_1PAD, 0x18),&lt;BR /&gt;0,0,0,&lt;/P&gt;&lt;P&gt;// 6 Reserved&lt;BR /&gt;0,0,0,0,&lt;/P&gt;&lt;P&gt;// 7 Reserved&lt;BR /&gt;0,0,0,0,&lt;/P&gt;&lt;P&gt;// 8 Reserved&lt;BR /&gt;0,0,0,0,&lt;/P&gt;&lt;P&gt;// 9 Page Program&lt;BR /&gt;FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x32, RADDR_SDR, FLEXSPI_1PAD, 0x18),&lt;BR /&gt;FLEXSPI_LUT_SEQ(WRITE_SDR, FLEXSPI_4PAD, 0x04, STOP, FLEXSPI_1PAD, 0),&lt;BR /&gt;0,0,&lt;/P&gt;&lt;P&gt;// 10 Reserved&lt;BR /&gt;0,0,0,0,&lt;/P&gt;&lt;P&gt;// 11 Chip Erase&lt;BR /&gt;FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xC7, STOP, FLEXSPI_1PAD, 0),&lt;BR /&gt;0,0,0,&lt;/P&gt;&lt;P&gt;// 12 Reserved&lt;BR /&gt;0,0,0,0,&lt;BR /&gt;},&lt;BR /&gt;},&lt;BR /&gt;.pageSize = 256u,&lt;BR /&gt;.sectorSize = 4u * 1024u,&lt;BR /&gt;.blockSize = 64u * 1024u,&lt;BR /&gt;.isUniformBlockSize = false,&lt;BR /&gt;};&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 09:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1475186#M191554</guid>
      <dc:creator>bjorns</dc:creator>
      <dc:date>2022-06-16T09:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1475620#M191573</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Firstly, I'd like to know the ratio of the phenomenon that arises, second, I'd highly recommend you to use the tool to verify the FlexSPI connection, meanwhile, you'd better check the hardware board, especially, the power supply circuit.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 01:30:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1475620#M191573</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-06-17T01:30:45Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1475751#M191583</link>
      <description>&lt;P&gt;Thanks for the answer.&lt;BR /&gt;&lt;BR /&gt;What tool are you referring to?&lt;BR /&gt;&lt;BR /&gt;The problems we are having is constant. It does not seem to change between runs.&lt;BR /&gt;&lt;BR /&gt;I will as our hardware designer to dubble check the flash power supply circuit.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;/Björn&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 06:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1475751#M191583</guid>
      <dc:creator>bjorns</dc:creator>
      <dc:date>2022-06-17T06:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1476405#M191632</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;The tool is the &lt;A href="https://github.com/JayHeng/NXP-MCUBootUtility" target="_self"&gt;NXP-MCUBootUtility&lt;/A&gt;, and I was wondering if you can update the schematic of the custom board.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 02:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1476405#M191632</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-06-20T02:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1478823#M191833</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Is there any way to send you the schematics privately?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;When it comes to point 3 above, I have tried to debug using SEGGERS Ozone tool and it seems to be lightning fast with the same binary. It seems that mcuxpresso has some issue handling large projects or I have some configuration somewhere that is wrong. Is this a knonw issue?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;/Björn&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 07:30:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1478823#M191833</guid>
      <dc:creator>bjorns</dc:creator>
      <dc:date>2022-06-23T07:30:34Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1479504#M191867</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;1) Is there any way to send you the schematics privately? &lt;BR /&gt;-- Maybe you can send a download link via the private message&lt;BR /&gt;1) Is this a knonw issue?&lt;BR /&gt;-- No.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jun 2022 03:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1479504#M191867</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-06-24T03:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1480337#M191936</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have got OK to post parts of the schematic. Let me know if this is enough.&lt;BR /&gt;&lt;BR /&gt;Thanks for your help.&lt;BR /&gt;/Björn&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 06:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1480337#M191936</guid>
      <dc:creator>bjorns</dc:creator>
      <dc:date>2022-06-27T06:58:20Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1480464#M191941</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;Actually, I've not found something wrong after checking the above picture, further, the Flash configuration is good.&lt;BR /&gt;Did you already use the NXP-MCUBootUtility for testing? Moreover, does it encounter a similar issue when debugging the demos from the SDK library for the RT106x?&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 09:14:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1480464#M191941</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-06-27T09:14:28Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1481264#M191982</link>
      <description>&lt;P&gt;I have been trying to get the NXP-MCUBoot utility to work but it refuses to connect over lpuart1. What test can it perform? I cant find anything about flash testing in the description of the tool.&lt;BR /&gt;&lt;BR /&gt;Yes, we see the same issues when debugging the the sdk examples.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;/Björn&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 14:20:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1481264#M191982</guid>
      <dc:creator>bjorns</dc:creator>
      <dc:date>2022-06-28T14:20:07Z</dc:date>
    </item>
    <item>
      <title>Re: RT1061 debugging issue (JLink)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1481499#M191997</link>
      <description>&lt;P&gt;Hi，&lt;BR /&gt;Thanks for your reply.&lt;BR /&gt;1) What test can it perform? I can't find anything about flash testing in the description of the tool.&lt;BR /&gt;-- During building connection with the NXP-MCUBoot utility, it will configure the external memory device, if it fails, it illustrates there's something wrong with the hardware.&lt;BR /&gt;Further, you can use either LPUART1 (GPIO_AD_B0_12 and GPIO_AD_B0_13)or USB OTG1 to connect the tool.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jun 2022 03:16:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1061-debugging-issue-JLink/m-p/1481499#M191997</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2022-06-29T03:16:42Z</dc:date>
    </item>
  </channel>
</rss>