<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: I.MX8MP MIPI CSI supported Data Types</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-MIPI-CSI-supported-Data-Types/m-p/1479822#M191888</link>
    <description>&lt;P&gt;Thank you Diana for clarifying this.&lt;/P&gt;</description>
    <pubDate>Fri, 24 Jun 2022 11:39:52 GMT</pubDate>
    <dc:creator>btogorean</dc:creator>
    <dc:date>2022-06-24T11:39:52Z</dc:date>
    <item>
      <title>I.MX8MP MIPI CSI supported Data Types</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-MIPI-CSI-supported-Data-Types/m-p/1477391#M191746</link>
      <description>&lt;P&gt;Hello NXP community,&lt;/P&gt;&lt;P&gt;I'm currently working on a Camera project based on I.MX8MP and the camera sensor is capable to ouput data in RAW16 format but is not clear for me if I.MX8MP can accept it.&lt;/P&gt;&lt;P&gt;In&amp;nbsp;Rev. 1, 06/2021&amp;nbsp;IMX8MPRM is stated that the ISI can store RAW16 at its output but on CSI only RAW6 to RAW14 are defined for input image data format.&lt;/P&gt;&lt;P&gt;So from my understanding is a limitation of CSI and RAW16 is not accepted as Data Type on MIPI. Is this correct or is there any way to capture RAW16 on I.MX8MP?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jun 2022 10:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-MIPI-CSI-supported-Data-Types/m-p/1477391#M191746</guid>
      <dc:creator>btogorean</dc:creator>
      <dc:date>2022-06-21T10:39:33Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MP MIPI CSI supported Data Types</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-MIPI-CSI-supported-Data-Types/m-p/1478078#M191789</link>
      <description>&lt;P&gt;Hi Bogdan,&lt;/P&gt;
&lt;P&gt;Your understanding is correct. Unfortunately there is a hardware limitation on MIPI CSI IP and it can support only up to RAW14 image format. Regarding why that format appears on ISI chapter, from what I can see ISI can either have as input the MIPI CSI interface or fetching the data from memory. I suppose the RAW16 image format can be used for memory to memory operations (not sure of this, I don't think it's implemented in software, but I can check) however, regarding capture it isn't possible.&lt;/P&gt;
&lt;P&gt;In fact, the same can go for ISP. The ISP actually does support RAW16, but it is not listed in&amp;nbsp;&lt;EM&gt;13.14.2.2.2 MIPI Inputs&amp;nbsp;&lt;/EM&gt;because MIPI-CSI does not support it and it's the only input.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Diana&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 09:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-MIPI-CSI-supported-Data-Types/m-p/1478078#M191789</guid>
      <dc:creator>dianapredescu</dc:creator>
      <dc:date>2022-06-22T09:04:01Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX8MP MIPI CSI supported Data Types</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-MIPI-CSI-supported-Data-Types/m-p/1479822#M191888</link>
      <description>&lt;P&gt;Thank you Diana for clarifying this.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jun 2022 11:39:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-MIPI-CSI-supported-Data-Types/m-p/1479822#M191888</guid>
      <dc:creator>btogorean</dc:creator>
      <dc:date>2022-06-24T11:39:52Z</dc:date>
    </item>
  </channel>
</rss>