<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Android 9 USB pendrive not detected in system level in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-9-USB-pendrive-not-detected-in-system-level/m-p/1479348#M191859</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Could you please share which i.MX6 are you using?&lt;BR /&gt;is it a custom board or an NXP board?&lt;BR /&gt;If possible, could you share the full logs?&lt;BR /&gt;&lt;BR /&gt;Also, please remember that if you're using i.MX6 SABRE Board the only USB supported should be the OTG one, and it is already defined at fstab.freescale:&lt;/P&gt;
&lt;P&gt;/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0*&amp;nbsp; auto auto defaults voldmanaged=usb:auto&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Thu, 23 Jun 2022 22:30:51 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-06-23T22:30:51Z</dc:date>
    <item>
      <title>Android 9 USB pendrive not detected in system level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-9-USB-pendrive-not-detected-in-system-level/m-p/1476830#M191687</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm using Android 9 in imx6 board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using USB H1 and defined in fstab.freescale.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1* auto auto defaults voldmanaged=usb:auto&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After boot If I insert pendrive its detected under &lt;STRONG&gt;/dev/block/sda1&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it not showing inside&amp;nbsp; &lt;STRONG&gt;/dev/block/vold/&amp;nbsp;&lt;/STRONG&gt;.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;So its not auto mounting also.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please help to fix it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aravinth&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 13:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-9-USB-pendrive-not-detected-in-system-level/m-p/1476830#M191687</guid>
      <dc:creator>aravinthkumarja</dc:creator>
      <dc:date>2022-06-20T13:13:30Z</dc:date>
    </item>
    <item>
      <title>Re: Android 9 USB pendrive not detected in system level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-9-USB-pendrive-not-detected-in-system-level/m-p/1479348#M191859</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Could you please share which i.MX6 are you using?&lt;BR /&gt;is it a custom board or an NXP board?&lt;BR /&gt;If possible, could you share the full logs?&lt;BR /&gt;&lt;BR /&gt;Also, please remember that if you're using i.MX6 SABRE Board the only USB supported should be the OTG one, and it is already defined at fstab.freescale:&lt;/P&gt;
&lt;P&gt;/devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0*&amp;nbsp; auto auto defaults voldmanaged=usb:auto&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 22:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-9-USB-pendrive-not-detected-in-system-level/m-p/1479348#M191859</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-06-23T22:30:51Z</dc:date>
    </item>
    <item>
      <title>Re: Android 9 USB pendrive not detected in system level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-9-USB-pendrive-not-detected-in-system-level/m-p/1480321#M191933</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have fixed the issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 06:37:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-9-USB-pendrive-not-detected-in-system-level/m-p/1480321#M191933</guid>
      <dc:creator>Aravinthkumar</dc:creator>
      <dc:date>2022-06-27T06:37:18Z</dc:date>
    </item>
  </channel>
</rss>