<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic android(Oreo) MIPI panel porting(IMX8MQEVK) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-Oreo-MIPI-panel-porting-IMX8MQEVK/m-p/1478258#M191805</link>
    <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I am porting the mipi dsi panel driver.&lt;/P&gt;&lt;P&gt;The cpu is imx8mq.&lt;/P&gt;&lt;P&gt;The driver code is using "panel-sn65dsix.c"&lt;/P&gt;&lt;P&gt;I have confirmed that it works in Oreo(imx_o8.1.0_1.3.0, kernel version is 4.9.78)&lt;/P&gt;&lt;P&gt;But, I need to upgrade the kernel version.&lt;/P&gt;&lt;P&gt;Currently, I am downloading "imx_o8.1.0_2.0.0" and working on porting it.(kernel version is 4.14.98)&lt;/P&gt;&lt;P&gt;However, driver porting failed.&lt;/P&gt;&lt;P&gt;The driver "sn65_panel_prove" seem to work, but it stop in the "sn65_panel_get_modes".&lt;/P&gt;&lt;P&gt;As a result of checking the kernel log, there is&lt;/P&gt;&lt;P&gt;"[drm] Cannot find any crtc or sizes",&amp;nbsp; "[drm] found mode none"&lt;/P&gt;&lt;P&gt;I think the drm sequence is different depending on the kernel version.&lt;/P&gt;&lt;P&gt;I attach the driver code and device tree file, I am using.&lt;/P&gt;&lt;P&gt;I need your help!!!&lt;/P&gt;&lt;P&gt;Thankyou!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 22 Jun 2022 14:58:50 GMT</pubDate>
    <dc:creator>dngnstjd</dc:creator>
    <dc:date>2022-06-22T14:58:50Z</dc:date>
    <item>
      <title>android(Oreo) MIPI panel porting(IMX8MQEVK)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-Oreo-MIPI-panel-porting-IMX8MQEVK/m-p/1478258#M191805</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I am porting the mipi dsi panel driver.&lt;/P&gt;&lt;P&gt;The cpu is imx8mq.&lt;/P&gt;&lt;P&gt;The driver code is using "panel-sn65dsix.c"&lt;/P&gt;&lt;P&gt;I have confirmed that it works in Oreo(imx_o8.1.0_1.3.0, kernel version is 4.9.78)&lt;/P&gt;&lt;P&gt;But, I need to upgrade the kernel version.&lt;/P&gt;&lt;P&gt;Currently, I am downloading "imx_o8.1.0_2.0.0" and working on porting it.(kernel version is 4.14.98)&lt;/P&gt;&lt;P&gt;However, driver porting failed.&lt;/P&gt;&lt;P&gt;The driver "sn65_panel_prove" seem to work, but it stop in the "sn65_panel_get_modes".&lt;/P&gt;&lt;P&gt;As a result of checking the kernel log, there is&lt;/P&gt;&lt;P&gt;"[drm] Cannot find any crtc or sizes",&amp;nbsp; "[drm] found mode none"&lt;/P&gt;&lt;P&gt;I think the drm sequence is different depending on the kernel version.&lt;/P&gt;&lt;P&gt;I attach the driver code and device tree file, I am using.&lt;/P&gt;&lt;P&gt;I need your help!!!&lt;/P&gt;&lt;P&gt;Thankyou!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 14:58:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-Oreo-MIPI-panel-porting-IMX8MQEVK/m-p/1478258#M191805</guid>
      <dc:creator>dngnstjd</dc:creator>
      <dc:date>2022-06-22T14:58:50Z</dc:date>
    </item>
  </channel>
</rss>