<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Android ADB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-ADB/m-p/1477886#M191777</link>
    <description>&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am running android on the imx8m plus evk. I want to use adb over ethernet. The issue i am running into is that android uses adb over usb. In order to switch that to ethernet, i need access to some kind of a local terminal. The terminal from the developer options is only showing in the search bar, but not in the actual settings. Sadly there is no appstore where i could get some kind of emulator.&lt;/P&gt;&lt;P&gt;please help^^&lt;/P&gt;&lt;P&gt;Moritz&lt;/P&gt;</description>
    <pubDate>Wed, 22 Jun 2022 06:29:02 GMT</pubDate>
    <dc:creator>Purdbull</dc:creator>
    <dc:date>2022-06-22T06:29:02Z</dc:date>
    <item>
      <title>Android ADB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-ADB/m-p/1477886#M191777</link>
      <description>&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am running android on the imx8m plus evk. I want to use adb over ethernet. The issue i am running into is that android uses adb over usb. In order to switch that to ethernet, i need access to some kind of a local terminal. The terminal from the developer options is only showing in the search bar, but not in the actual settings. Sadly there is no appstore where i could get some kind of emulator.&lt;/P&gt;&lt;P&gt;please help^^&lt;/P&gt;&lt;P&gt;Moritz&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 06:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-ADB/m-p/1477886#M191777</guid>
      <dc:creator>Purdbull</dc:creator>
      <dc:date>2022-06-22T06:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: Android ADB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-ADB/m-p/1480594#M191947</link>
      <description>&lt;P&gt;pls refer to the similar topic and document as below:&lt;/P&gt;
&lt;P&gt;“&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enable-Ethernet-for-Android-Auto-with-mek-8q/ta-p/1100866”" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Enable-Ethernet-for-Android-Auto-with-mek-8q/ta-p/1100866”&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;“&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-EVK-ADB-over-network-debug-Android-studio-Install/m-p/1210358”" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-EVK-ADB-over-network-debug-Android-studio-Install/m-p/1210358”&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;“&lt;A href="https://stackoverflow.com/questions/2604727/how-can-i-connect-to-android-with-adb-over-tcp”" target="_blank"&gt;https://stackoverflow.com/questions/2604727/how-can-i-connect-to-android-with-adb-over-tcp”&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 12:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-ADB/m-p/1480594#M191947</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2022-06-27T12:48:38Z</dc:date>
    </item>
  </channel>
</rss>