<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Imx8 SCFW entry point question in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Imx8-SCFW-entry-point-question/m-p/1477010#M191705</link>
    <description>&lt;P&gt;Hello, &lt;BR /&gt;&lt;BR /&gt;Yes it has, you may refer to the reference manual chapter 5.9.4 High Level Container Format &amp;amp; 5.9.4.3 How the SCU ROM Parses Offsets/Addresses in the Image Container &lt;BR /&gt;&lt;BR /&gt;Best regards, &lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Tue, 21 Jun 2022 00:41:43 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-06-21T00:41:43Z</dc:date>
    <item>
      <title>Imx8 SCFW entry point question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx8-SCFW-entry-point-question/m-p/1460037#M190533</link>
      <description>&lt;P&gt;Quick question if anyone knows... Does the SCFW have the standard entry point in the firmware (scfw_tcm.bin) as any other Cortex-m4?&amp;nbsp; This would be having the initial stack pointer address stored at 0x0 and the initial program counter at 0x4 of the binary.&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 13:05:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx8-SCFW-entry-point-question/m-p/1460037#M190533</guid>
      <dc:creator>bghiggins</dc:creator>
      <dc:date>2022-05-18T13:05:33Z</dc:date>
    </item>
    <item>
      <title>Re: Imx8 SCFW entry point question</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx8-SCFW-entry-point-question/m-p/1477010#M191705</link>
      <description>&lt;P&gt;Hello, &lt;BR /&gt;&lt;BR /&gt;Yes it has, you may refer to the reference manual chapter 5.9.4 High Level Container Format &amp;amp; 5.9.4.3 How the SCU ROM Parses Offsets/Addresses in the Image Container &lt;BR /&gt;&lt;BR /&gt;Best regards, &lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jun 2022 00:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx8-SCFW-entry-point-question/m-p/1477010#M191705</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-06-21T00:41:43Z</dc:date>
    </item>
  </channel>
</rss>