<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Xen hypervisor</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1476901#M191696</link>
    <description>&lt;P&gt;Hi&amp;nbsp; &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198291"&gt;@Chandrakanth_S_O&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finally I've got it working on 5.4.70. Unfortunatelly I didn't get any response from NXP. I've started to go back in versions and also inspecting the imx-xen code belonging to each of those versions, and finally I've got 5.4.70 working with a Dom0 and DomU. So far just statarted two Qt basic aplications on each running Linux to test if both displays (one for each Linux are running) and indeed they are. My next step will be to use the can interface directly in Linux in Dom=, because I think currently it is asigned to the M4. So I could say I was sucess in the basic demo with Xen.&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jun 2022 15:29:22 GMT</pubDate>
    <dc:creator>albfon</dc:creator>
    <dc:date>2022-06-20T15:29:22Z</dc:date>
    <item>
      <title>Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1430479#M188348</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We are working on validate xen with 8qm Mek facing below issues&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. DISTRO_FEATURES_append = " xen"&lt;BR /&gt;made changes in the local.config to enable xen but could not find spl-imx8qm-xen.bin, rootfs.sdcard and u-boot-imx8qm-xen-dom0.imx are not generated&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. sudo dd if=fsl-image-validation-imx-imx8qxpc0mek.sdcard of=/dev/sdb bs=1M status=progress&lt;BR /&gt;we used this command to copy to sdcard to create partition and copy the images.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3. while we stop at bootloader and give the command " run xenmmcboot " we are getting the following error&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt; run xenmmcboot&lt;BR /&gt;136190 bytes read in 9 ms (14.4 MiB/s)&lt;BR /&gt;106496 bytes read in 7 ms (14.5 MiB/s)&lt;BR /&gt;Loading hdp firmware from 0x000000009c000000 offset 0x0000000000002000&lt;BR /&gt;Loading hdp firmware Complete&lt;BR /&gt;28013056 bytes read in 136 ms (196.4 MiB/s)&lt;BR /&gt;Bad Linux ARM64 Image magic!&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;Can you let us know how to do the three partition for xen on sd card , and build the rootfs.sdcard image&lt;BR /&gt;how to make sure xen is enabled or not&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Mar 2022 04:49:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1430479#M188348</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2022-03-18T04:49:17Z</dc:date>
    </item>
    <item>
      <title>Re: Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1431201#M188420</link>
      <description>&lt;P&gt;Which bsp are you using?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 09:34:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1431201#M188420</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2022-03-21T09:34:40Z</dc:date>
    </item>
    <item>
      <title>Re: Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1431586#M188446</link>
      <description>&lt;P&gt;thanks &lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788" target="_self"&gt;&lt;SPAN class=""&gt;nxf65025&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;for the response. we tried recent 5.10.72 as well as older release too. Is xen supported by the prebuilt binaries from NXP? We are seeing three partitions need to be created with 1 FAT and remaining two for the respective OS but guides doesnt have those steps mentioned. pls suggest&lt;/P&gt;</description>
      <pubDate>Tue, 22 Mar 2022 03:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1431586#M188446</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2022-03-22T03:01:19Z</dc:date>
    </item>
    <item>
      <title>Re: Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1470556#M191271</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/65315" target="_self"&gt;&lt;SPAN class=""&gt;vinothkumars&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Did you have any sucess on this? I have started to test xen on imx8QM and I've got stuck more or less at the same points than you. I'm using Linux 5.10.52 because is the last one whose documentation mention about xen virtualization. From that one on, NXP doc just mention jailhouse. Anyways I wasn't sucesfull by testing this.&lt;/P&gt;&lt;P&gt;Did you make any progress?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 09:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1470556#M191271</guid>
      <dc:creator>albfon</dc:creator>
      <dc:date>2022-06-08T09:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1476528#M191649</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/1477"&gt;@albfon&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;I too have same problem with Xen. I received reply from nxp regarding xen that it doesn't work with 5.0, 5.4 and 5.10. they asked me to migrate to 5.15 or stay in 4.14. Let me know if you get Xen working.&lt;/P&gt;&lt;P&gt;regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 06:31:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1476528#M191649</guid>
      <dc:creator>Chandrakanth_S_O</dc:creator>
      <dc:date>2022-06-20T06:31:53Z</dc:date>
    </item>
    <item>
      <title>Re: Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1476901#M191696</link>
      <description>&lt;P&gt;Hi&amp;nbsp; &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198291"&gt;@Chandrakanth_S_O&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finally I've got it working on 5.4.70. Unfortunatelly I didn't get any response from NXP. I've started to go back in versions and also inspecting the imx-xen code belonging to each of those versions, and finally I've got 5.4.70 working with a Dom0 and DomU. So far just statarted two Qt basic aplications on each running Linux to test if both displays (one for each Linux are running) and indeed they are. My next step will be to use the can interface directly in Linux in Dom=, because I think currently it is asigned to the M4. So I could say I was sucess in the basic demo with Xen.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 15:29:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1476901#M191696</guid>
      <dc:creator>albfon</dc:creator>
      <dc:date>2022-06-20T15:29:22Z</dc:date>
    </item>
    <item>
      <title>Re: Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1483666#M192135</link>
      <description>&lt;P&gt;5.15 not have xen support.&lt;/P&gt;</description>
      <pubDate>Sun, 03 Jul 2022 11:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1483666#M192135</guid>
      <dc:creator>Peng_Fan</dc:creator>
      <dc:date>2022-07-03T11:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1535302#M196192</link>
      <description>Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/1477"&gt;@albfon&lt;/a&gt;&lt;BR /&gt;what is the bitbake command you gave after enabling xen and what all images are generated.&lt;BR /&gt;Can you please elaborate little more on the build and flash procedure please</description>
      <pubDate>Tue, 11 Oct 2022 05:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/1535302#M196192</guid>
      <dc:creator>swapna</dc:creator>
      <dc:date>2022-10-11T05:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: Xen hypervisor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/2093638#M237040</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/1477"&gt;@albfon&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;Thanks for sharing your success with Xen on 5.4.70.&amp;nbsp;Could you please share the steps or modifications you made to successfully integrate Xen on i.MX with that kernel version? Especially any changes to the device tree, Xen recipe, or Yocto build settings would be really helpful.&lt;/P&gt;&lt;P&gt;Any guidance or reference would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 08 May 2025 12:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-hypervisor/m-p/2093638#M237040</guid>
      <dc:creator>Avani_b_Nair</dc:creator>
      <dc:date>2025-05-08T12:00:01Z</dc:date>
    </item>
  </channel>
</rss>