<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8MP EVK v4l2-ctl (v4l-utils) missing?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EVK-v4l2-ctl-v4l-utils-missing/m-p/1476832#M191688</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202502"&gt;@mihael0010&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;You can add v4l-utils by yourselves by putting following line into &lt;EM&gt;&amp;lt;yocto-bsp&amp;gt;/build-xwayland/conf/local.conf&lt;/EM&gt; :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;IMAGE_INSTALL_append = " v4l-utils"&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;K&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jun 2022 13:22:40 GMT</pubDate>
    <dc:creator>khang_letruong</dc:creator>
    <dc:date>2022-06-20T13:22:40Z</dc:date>
    <item>
      <title>i.MX8MP EVK v4l2-ctl (v4l-utils) missing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EVK-v4l2-ctl-v4l-utils-missing/m-p/1476820#M191684</link>
      <description>&lt;P&gt;we have i.MX 8M PLUS EVK and we are doing an image sensor driver, I flashed the sd card as follows:&lt;BR /&gt;1.)&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;DISTRO=fsl-imx-wayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;2.)&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;bitbake imx-image-full&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;3.)&lt;/P&gt;&lt;LI-CODE lang="c"&gt;bzcat imx-image-full-imx8mp-lpddr4-evk.wic.bz2 | sudo dd of=/dev/sdd bs=1M conv=fsync&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After flashing to the SD card, the system starts normally, but when I type the command:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;v4l2-ctl --list-devices&lt;/LI-CODE&gt;&lt;P&gt;the error "&lt;STRONG&gt;v4l2-ctl: command not found&lt;/STRONG&gt;" appears!&lt;/P&gt;&lt;P&gt;Why v4l-utils is not installed on imx-image-full?&lt;/P&gt;&lt;P&gt;ps*** First I put imx-image-multimedia, so after that I put imx-image-full because I thought it would help, but nothing&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 12:38:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EVK-v4l2-ctl-v4l-utils-missing/m-p/1476820#M191684</guid>
      <dc:creator>mihael0010</dc:creator>
      <dc:date>2022-06-20T12:38:00Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP EVK v4l2-ctl (v4l-utils) missing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EVK-v4l2-ctl-v4l-utils-missing/m-p/1476832#M191688</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202502"&gt;@mihael0010&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;You can add v4l-utils by yourselves by putting following line into &lt;EM&gt;&amp;lt;yocto-bsp&amp;gt;/build-xwayland/conf/local.conf&lt;/EM&gt; :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;IMAGE_INSTALL_append = " v4l-utils"&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;K&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 13:22:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EVK-v4l2-ctl-v4l-utils-missing/m-p/1476832#M191688</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2022-06-20T13:22:40Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP EVK v4l2-ctl (v4l-utils) missing?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EVK-v4l2-ctl-v4l-utils-missing/m-p/1477229#M191728</link>
      <description>&lt;P&gt;Super thanks &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;only the syntax is:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;IMAGE_INSTALL:append = " v4l-utils"&lt;/LI-CODE&gt;</description>
      <pubDate>Tue, 21 Jun 2022 07:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-EVK-v4l2-ctl-v4l-utils-missing/m-p/1477229#M191728</guid>
      <dc:creator>mihael0010</dc:creator>
      <dc:date>2022-06-21T07:13:56Z</dc:date>
    </item>
  </channel>
</rss>