<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT117x: ADIN protection in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT117x-ADIN-protection/m-p/1476722#M191669</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Does the analog input pin with&lt;BR /&gt;&amp;nbsp;&amp;nbsp; VREFH = 1.8V,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; CSACAL = 1 and&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 3V3 GPIO_NVCC mode&lt;BR /&gt;need a protection against voltage levels above 1.8V or is a protection for values above 3.96V sufficient?&lt;/P&gt;&lt;P&gt;Thanks for the help!&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jun 2022 10:30:24 GMT</pubDate>
    <dc:creator>ak2</dc:creator>
    <dc:date>2022-06-20T10:30:24Z</dc:date>
    <item>
      <title>RT117x: ADIN protection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT117x-ADIN-protection/m-p/1476722#M191669</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Does the analog input pin with&lt;BR /&gt;&amp;nbsp;&amp;nbsp; VREFH = 1.8V,&lt;BR /&gt;&amp;nbsp;&amp;nbsp; CSACAL = 1 and&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 3V3 GPIO_NVCC mode&lt;BR /&gt;need a protection against voltage levels above 1.8V or is a protection for values above 3.96V sufficient?&lt;/P&gt;&lt;P&gt;Thanks for the help!&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 10:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT117x-ADIN-protection/m-p/1476722#M191669</guid>
      <dc:creator>ak2</dc:creator>
      <dc:date>2022-06-20T10:30:24Z</dc:date>
    </item>
    <item>
      <title>Re: RT117x: ADIN protection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT117x-ADIN-protection/m-p/1477105#M191712</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/119027"&gt;@ak2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;From the RT1170RM, we can know some information:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1655780263059.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183966iD4B952E01BA91698/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1655780263059.png" alt="kerryzhou_0-1655780263059.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;But, if you define&amp;nbsp;&lt;SPAN&gt;CSACAL = 1, then it is&amp;nbsp;Full scale (Factor of 1),&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_1-1655780300878.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183967iDA728FC6B4358213/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_1-1655780300878.png" alt="kerryzhou_1-1655780300878.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, the input voltage should follow this table:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_2-1655780440844.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183968i4D6A6F49922578A5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_2-1655780440844.png" alt="kerryzhou_2-1655780440844.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;can't above 1.8V, thanks.&lt;/P&gt;
&lt;P&gt;If the&amp;nbsp;&lt;SPAN&gt;CSACAL = 0, you can input 3.3V.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jun 2022 03:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT117x-ADIN-protection/m-p/1477105#M191712</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2022-06-21T03:01:47Z</dc:date>
    </item>
    <item>
      <title>Re: RT117x: ADIN protection</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT117x-ADIN-protection/m-p/1477456#M191750</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;As you mention, I will set CSCALE to 0.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jun 2022 12:42:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT117x-ADIN-protection/m-p/1477456#M191750</guid>
      <dc:creator>ak2</dc:creator>
      <dc:date>2022-06-21T12:42:17Z</dc:date>
    </item>
  </channel>
</rss>