<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.MX35 IIM SCS register in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX35-IIM-SCS-register/m-p/237605#M19166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem is resolved in further Linux versions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.11.1 is one of these working kernels&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Oct 2013 11:37:22 GMT</pubDate>
    <dc:creator>maxvankessel</dc:creator>
    <dc:date>2013-10-14T11:37:22Z</dc:date>
    <item>
      <title>I.MX35 IIM SCS register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX35-IIM-SCS-register/m-p/237604#M19165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to read a byte from register IIMSCS2,&lt;/P&gt;&lt;P&gt;But every time I try the kernel get stuck.&lt;/P&gt;&lt;P&gt;Other registers like IIMSREV are readable but I can't read IIMSCS0&amp;nbsp; to IIMSCS3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Linux 3.2 on a I.MX35 and some hardware bits are signed in this register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Code: &lt;/P&gt;&lt;P&gt;&lt;EM&gt; u8 rev = (__raw_readb(MX35_IO_ADDRESS(MX35_IIM_BASE_ADDR + MXC_IIMSCS2))) &amp;amp; 0x7F;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got a succesfull result in previous kernel 2.6.28 and 2.6.31.&lt;/P&gt;&lt;P&gt;With this code:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; unsigned char *iim_base;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; unsigned char&amp;nbsp; reg;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; iim_base = ioremap(IIM_BASE_ADDR, SZ_4K);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; reg = *(iim_base + IIM_SCS2_OFFSET);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; iounmap(iim_base);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; u8 rev = reg &amp;amp; IIM_SCS_DATA_MASK; // 0x7F&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also this piece of code ain't working for kernel 3.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone explain this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2013 22:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX35-IIM-SCS-register/m-p/237604#M19165</guid>
      <dc:creator>maxvankessel</dc:creator>
      <dc:date>2013-09-17T22:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX35 IIM SCS register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX35-IIM-SCS-register/m-p/237605#M19166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem is resolved in further Linux versions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.11.1 is one of these working kernels&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Oct 2013 11:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX35-IIM-SCS-register/m-p/237605#M19166</guid>
      <dc:creator>maxvankessel</dc:creator>
      <dc:date>2013-10-14T11:37:22Z</dc:date>
    </item>
  </channel>
</rss>