<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Nodejs do_compile fails. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Nodejs-do-compile-fails/m-p/1476115#M191609</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm a bit new to creating images so I'm running into multiple errors which I have been resolving.&amp;nbsp; Now, I have run into an error that I can't resolve.&lt;/P&gt;&lt;P&gt;Host Machine is running Ubuntu 20.04&lt;/P&gt;&lt;P&gt;Target machine is imx8 mini.&lt;/P&gt;&lt;P&gt;distro is fsl_imx_xwayland&lt;/P&gt;&lt;P&gt;machine is imx8mevk&lt;/P&gt;&lt;P&gt;image is imx_image_multimedia.&lt;/P&gt;&lt;P&gt;I was able to create the image successfully without nodejs.&lt;/P&gt;&lt;P&gt;When I try to create same image but adding IMAGE_INSTALL:append = " nodejs" to local.conf the compilation fails with exit code "1".&amp;nbsp; Same error if I attempt to compile nodejs recipe by itself.&lt;/P&gt;&lt;P&gt;the bb file indicates that the nodejs version is 16.11.1.&lt;/P&gt;&lt;P&gt;Any ideas on how to resolve this issue?&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 17 Jun 2022 16:33:32 GMT</pubDate>
    <dc:creator>MginoM</dc:creator>
    <dc:date>2022-06-17T16:33:32Z</dc:date>
    <item>
      <title>Nodejs do_compile fails.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nodejs-do-compile-fails/m-p/1476115#M191609</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm a bit new to creating images so I'm running into multiple errors which I have been resolving.&amp;nbsp; Now, I have run into an error that I can't resolve.&lt;/P&gt;&lt;P&gt;Host Machine is running Ubuntu 20.04&lt;/P&gt;&lt;P&gt;Target machine is imx8 mini.&lt;/P&gt;&lt;P&gt;distro is fsl_imx_xwayland&lt;/P&gt;&lt;P&gt;machine is imx8mevk&lt;/P&gt;&lt;P&gt;image is imx_image_multimedia.&lt;/P&gt;&lt;P&gt;I was able to create the image successfully without nodejs.&lt;/P&gt;&lt;P&gt;When I try to create same image but adding IMAGE_INSTALL:append = " nodejs" to local.conf the compilation fails with exit code "1".&amp;nbsp; Same error if I attempt to compile nodejs recipe by itself.&lt;/P&gt;&lt;P&gt;the bb file indicates that the nodejs version is 16.11.1.&lt;/P&gt;&lt;P&gt;Any ideas on how to resolve this issue?&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 16:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nodejs-do-compile-fails/m-p/1476115#M191609</guid>
      <dc:creator>MginoM</dc:creator>
      <dc:date>2022-06-17T16:33:32Z</dc:date>
    </item>
  </channel>
</rss>