<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: An error is always reported when loading .ko files in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/An-error-is-always-reported-when-loading-ko-files/m-p/1476069#M191606</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202401"&gt;@mine233&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Looks like the USB driver was not built with the same source (and same configuration such as debug enabled/disabled ...) of running kernel or USB driver had been built at a moment before the running kernel was (re-)built.&lt;/P&gt;</description>
    <pubDate>Fri, 17 Jun 2022 14:44:39 GMT</pubDate>
    <dc:creator>khang_letruong</dc:creator>
    <dc:date>2022-06-17T14:44:39Z</dc:date>
    <item>
      <title>An error is always reported when loading .ko files</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/An-error-is-always-reported-when-loading-ko-files/m-p/1475693#M191579</link>
      <description>&lt;P&gt;I want to load the USB driver separately, so I take out the usb_wwan.c&amp;nbsp; and option.c in imx-linux-kernel separately and compile them into modules. After normal compilation, .ko files can be generated, but errors are always reported when insmod is on the development board.&lt;/P&gt;&lt;P&gt;1.Error message of dmesg:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mine233_0-1655437023667.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183688i48B70A742BB4E24F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mine233_0-1655437023667.png" alt="mine233_0-1655437023667.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mine233_0-1655437023667.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2.Kernel version of the development board:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mine233_1-1655437094278.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183689i6BE08207ED45E8F2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mine233_1-1655437094278.png" alt="mine233_1-1655437094278.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mine233_1-1655437094278.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3.The Linux kernel version I downloaded from the IMX server is also IMX_ 5.4.70_ 2.3.0&lt;/P&gt;&lt;P&gt;4.The cross compiler uses gcc-arm-9.2-2019.12-x86_ 64-aarch64-none-linux-gnu. tar. xz&lt;/P&gt;&lt;P&gt;How to solve this problem&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 03:44:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/An-error-is-always-reported-when-loading-ko-files/m-p/1475693#M191579</guid>
      <dc:creator>mine233</dc:creator>
      <dc:date>2022-06-17T03:44:51Z</dc:date>
    </item>
    <item>
      <title>Re: An error is always reported when loading .ko files</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/An-error-is-always-reported-when-loading-ko-files/m-p/1476069#M191606</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202401"&gt;@mine233&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Looks like the USB driver was not built with the same source (and same configuration such as debug enabled/disabled ...) of running kernel or USB driver had been built at a moment before the running kernel was (re-)built.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 14:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/An-error-is-always-reported-when-loading-ko-files/m-p/1476069#M191606</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2022-06-17T14:44:39Z</dc:date>
    </item>
  </channel>
</rss>