<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RCU stall on kernel 4.4.240</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RCU-stall-on-kernel-4-4-240/m-p/1474603#M191524</link>
    <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&amp;nbsp; but there is some similar bug? if yes can you share some details for identify the issue root cause?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 16:02:48 GMT</pubDate>
    <dc:creator>ivang</dc:creator>
    <dc:date>2022-06-15T16:02:48Z</dc:date>
    <item>
      <title>RCU stall on kernel 4.4.240</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RCU-stall-on-kernel-4-4-240/m-p/1469398#M191191</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am getting occasionally kernels hanging (sometimes hours after boot) with the following output occurring and that just goes on until i reboot the machine:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;INFO: rcu_sched self-detected stall on CPU
1-...: (52300 ticks this GP) idle=439/140000000000001/0 softirq=806264/806264 fqs=52291
INFO: rcu_sched detected stalls on CPUs/tasks:
1-...: (52300 ticks this GP) idle=439/140000000000001/0 softirq=806264/806264 fqs=52291
(detected by 0, t=52542 jiffies, g=463552, c=463551, q=391502)
Task dump for CPU 1:
WQ#1(System) R running 4640 28173 28140 0x00000002
Backtrace:
[&amp;lt;beb5bd7c&amp;gt;] (0xbeb5bd7c) from [&amp;lt;beb5bdac&amp;gt;] (0xbeb5bdac)
Backtrace aborted due to bad frame pointer &amp;lt;8007759c&amp;gt;
(t=52545 jiffies g=463552 c=463551 q=391595)
Task dump for CPU 1:
WQ#1(System) R running 4640 28173 28140 0x00000002
Backtrace:
[&amp;lt;80014a38&amp;gt;] (dump_backtrace) from [&amp;lt;80014c80&amp;gt;] (show_stack+0x20/0x24)
r7:807b26c0 r6:60010193 r5:807b26c0 r4:bcfbae00
[&amp;lt;80014c60&amp;gt;] (show_stack) from [&amp;lt;80057204&amp;gt;] (sched_show_task+0xbc/0x118)
[&amp;lt;80057148&amp;gt;] (sched_show_task) from [&amp;lt;80059354&amp;gt;] (dump_cpu_task+0x3c/0x4c)
r5:807b26c0 r4:00000001
[&amp;lt;80059318&amp;gt;] (dump_cpu_task) from [&amp;lt;80082344&amp;gt;] (rcu_dump_cpu_stacks+0x94/0xd8)
r5:807b26c0 r4:00000001
[&amp;lt;800822b0&amp;gt;] (rcu_dump_cpu_stacks) from [&amp;lt;80086698&amp;gt;] (rcu_check_callbacks+0x548/0x860)
r9:bf7d3100 r8:807b26c0 r7:807a460c r6:3f033000 r5:807a4584 r4:807a0100
[&amp;lt;80086150&amp;gt;] (rcu_check_callbacks) from [&amp;lt;8008aca4&amp;gt;] (update_process_times+0x48/0xa8)
r10:8009d204 r9:bf7cfc98 r8:805989c4 r7:00002fd9 r6:bcfbae00 r5:ffffe000
r4:00000000
[&amp;lt;8008ac5c&amp;gt;] (update_process_times) from [&amp;lt;8009d200&amp;gt;] (tick_sched_handle+0x58/0x5c)
r7:00002fd9 r6:23800e91 r5:beb5bde8 r4:bf7cfdb8
[&amp;lt;8009d1a8&amp;gt;] (tick_sched_handle) from [&amp;lt;8009d258&amp;gt;] (tick_sched_timer+0x54/0x9c)
[&amp;lt;8009d204&amp;gt;] (tick_sched_timer) from [&amp;lt;8008b9fc&amp;gt;] (__hrtimer_run_queues+0x160/0x324)
r7:bf7cfc00 r6:beb5a000 r5:00000000 r4:bf7cfdb8
[&amp;lt;8008b89c&amp;gt;] (__hrtimer_run_queues) from [&amp;lt;8008c2e8&amp;gt;] (hrtimer_interrupt+0xc8/0x22c)
r10:bf7cfc78 r9:bf7cfc98 r8:bf7cfc14 r7:00000000 r6:8079cc00 r5:00000003
r4:bf7cfc00
[&amp;lt;8008c220&amp;gt;] (hrtimer_interrupt) from [&amp;lt;80018728&amp;gt;] (twd_handler+0x3c/0x50)
r10:807eea3c r9:f4000100 r8:bf022d80 r7:00000010 r6:bf7d5700 r5:bf08a400
r4:00000001
[&amp;lt;800186ec&amp;gt;] (twd_handler) from [&amp;lt;8007c1e8&amp;gt;] (handle_percpu_devid_irq+0x88/0x1a0)
r5:bf08a400 r4:8079e38c
[&amp;lt;8007c160&amp;gt;] (handle_percpu_devid_irq) from [&amp;lt;8007759c&amp;gt;] (generic_handle_irq+0x30/0x44)
r10:807a4cc0 r9:f4000100 r8:bf034000 r7:00000001 r6:00000000 r5:00000010
r4:8079e38c r3:8007c160
[&amp;lt;8007756c&amp;gt;] (generic_handle_irq) from [&amp;lt;800778a0&amp;gt;] (__handle_domain_irq+0x60/0xc8)
[&amp;lt;80077840&amp;gt;] (__handle_domain_irq) from [&amp;lt;800094c0&amp;gt;] (gic_handle_irq+0x60/0xc4)
r9:f4000100 r8:807eea38 r7:beb5bde8 r6:000003ff r5:000003eb r4:f400010c
[&amp;lt;80009460&amp;gt;] (gic_handle_irq) from [&amp;lt;80593534&amp;gt;] (__irq_svc+0x54/0x70)
Exception stack(0xbeb5bde8 to 0xbeb5be30)
bde0: bf1a1e44 00000000 0000b2cc 0000a7b4 00000000 00000000
be00: ffffffff 01bc9294 bf1a1e40 bf1a1e40 00000001 beb5be44 80592d34 beb5be38
be20: 8009ef44 80592d60 80010013 ffffffff
r10:00000001 r9:bf1a1e40 r8:bf1a1e40 r7:beb5be1c r6:ffffffff r5:80010013
r4:80592d60
[&amp;lt;80592d20&amp;gt;] (_raw_spin_lock) from [&amp;lt;8009ef44&amp;gt;] (futex_wake+0xa4/0x194)
[&amp;lt;8009eea0&amp;gt;] (futex_wake) from [&amp;lt;800a0ec4&amp;gt;] (do_futex+0x128/0xd80)
r10:000000f0 r9:01bc9294 r8:00000001 r7:01bc9294 r6:00000081 r5:00000000
r4:00000000
[&amp;lt;800a0d9c&amp;gt;] (do_futex) from [&amp;lt;800a1ba4&amp;gt;] (SyS_futex+0x88/0x188)
r10:000000f0 r9:beb5a000 r8:80010844 r7:01bc9294 r6:00000081 r5:00000000
r4:00000001
[&amp;lt;800a1b1c&amp;gt;] (SyS_futex) from [&amp;lt;80010660&amp;gt;] (ret_fast_syscall+0x0/0x48)
r10:000000f0 r9:beb5a000 r8:80010844 r7:000000f0 r6:7ee2e842 r5:01bc92b0
r4:00000000&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There doesn't appear to be any pattern, when it occurs and I cannot reproduce it. Any ideas on how to debug this issue?&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Ivan&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 10:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RCU-stall-on-kernel-4-4-240/m-p/1469398#M191191</guid>
      <dc:creator>ivang</dc:creator>
      <dc:date>2022-06-07T10:24:41Z</dc:date>
    </item>
    <item>
      <title>Re: RCU stall on kernel 4.4.240</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RCU-stall-on-kernel-4-4-240/m-p/1473775#M191479</link>
      <description>&lt;P&gt;Please try the newer release of BSP.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 16:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RCU-stall-on-kernel-4-4-240/m-p/1473775#M191479</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2022-06-14T16:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: RCU stall on kernel 4.4.240</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RCU-stall-on-kernel-4-4-240/m-p/1474603#M191524</link>
      <description>&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&amp;nbsp; but there is some similar bug? if yes can you share some details for identify the issue root cause?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 16:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RCU-stall-on-kernel-4-4-240/m-p/1474603#M191524</guid>
      <dc:creator>ivang</dc:creator>
      <dc:date>2022-06-15T16:02:48Z</dc:date>
    </item>
  </channel>
</rss>