<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX-8ULP HiFi4 On-chip Memory in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8ULP-HiFi4-On-chip-Memory/m-p/1474547#M191523</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;My understanding is that the HiFi4 in the&amp;nbsp;iMX-8ULP has the following:&lt;/P&gt;&lt;P&gt;- 64KB of ITCM and 64KB of DTCM which I am guessing are zero wait state.&lt;/P&gt;&lt;P&gt;-32KB DCache and 32KB ICache.&lt;/P&gt;&lt;P&gt;Please confirm these numbers. I think it also has an additional amount of on-chip memory that is available for the HiFi4 to use.&lt;/P&gt;&lt;P&gt;Could you confirm what the size of the additional memory and the number of wait states are?&lt;/P&gt;&lt;P&gt;Is this on-chip memory shared with other processors (M33?)?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 14:41:33 GMT</pubDate>
    <dc:creator>caguilar10</dc:creator>
    <dc:date>2022-06-15T14:41:33Z</dc:date>
    <item>
      <title>iMX-8ULP HiFi4 On-chip Memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-8ULP-HiFi4-On-chip-Memory/m-p/1474547#M191523</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;My understanding is that the HiFi4 in the&amp;nbsp;iMX-8ULP has the following:&lt;/P&gt;&lt;P&gt;- 64KB of ITCM and 64KB of DTCM which I am guessing are zero wait state.&lt;/P&gt;&lt;P&gt;-32KB DCache and 32KB ICache.&lt;/P&gt;&lt;P&gt;Please confirm these numbers. I think it also has an additional amount of on-chip memory that is available for the HiFi4 to use.&lt;/P&gt;&lt;P&gt;Could you confirm what the size of the additional memory and the number of wait states are?&lt;/P&gt;&lt;P&gt;Is this on-chip memory shared with other processors (M33?)?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 14:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-8ULP-HiFi4-On-chip-Memory/m-p/1474547#M191523</guid>
      <dc:creator>caguilar10</dc:creator>
      <dc:date>2022-06-15T14:41:33Z</dc:date>
    </item>
  </channel>
</rss>