<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMXRT1050 USB Host in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-USB-Host/m-p/1474196#M191506</link>
    <description>&lt;P&gt;Hello I am trying to use VCOM slave device with IMXRT1050-EVKB. IMXRT1050-EVKB will be host and receive data from slave. My goal is to be able to receive and process the data sent by the slave device via USB. I am not looking for an complete USB software.&lt;/P&gt;&lt;P&gt;I examined "host_cdc" example and not understand how it works and transmit-receive data. Try to use peripheral tool for get some hint but also not worked. I read documentation of usb via peripheral tool. I did not see USB section at sdk documentation.&lt;/P&gt;&lt;P&gt;My question is how can I receive-transmit data via USB like UART?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Kaan.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 07:11:24 GMT</pubDate>
    <dc:creator>omerkaanbasakin</dc:creator>
    <dc:date>2022-06-15T07:11:24Z</dc:date>
    <item>
      <title>IMXRT1050 USB Host</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-USB-Host/m-p/1474196#M191506</link>
      <description>&lt;P&gt;Hello I am trying to use VCOM slave device with IMXRT1050-EVKB. IMXRT1050-EVKB will be host and receive data from slave. My goal is to be able to receive and process the data sent by the slave device via USB. I am not looking for an complete USB software.&lt;/P&gt;&lt;P&gt;I examined "host_cdc" example and not understand how it works and transmit-receive data. Try to use peripheral tool for get some hint but also not worked. I read documentation of usb via peripheral tool. I did not see USB section at sdk documentation.&lt;/P&gt;&lt;P&gt;My question is how can I receive-transmit data via USB like UART?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Kaan.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 07:11:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-USB-Host/m-p/1474196#M191506</guid>
      <dc:creator>omerkaanbasakin</dc:creator>
      <dc:date>2022-06-15T07:11:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1050 USB Host</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-USB-Host/m-p/1475701#M191581</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The host CDC project is a simple demonstration program. It enumerates a COM port and echoes back the data from the UART as follows.&lt;/P&gt;
&lt;P&gt;1.The host CDC receives data from the UART, which is plugged in the PC. Type characters in the terminal tool, such&amp;nbsp;as Tera Term, and the characters are sent to the host example.&lt;BR /&gt;2. After the host example receives data from the UART, it sends the data to the device virtual COM.&lt;BR /&gt;3. After the data has been sent to the device virtual COM successfully, it receives the same data from the device virtual&amp;nbsp;COM.&lt;BR /&gt;4. If the host has received the data, it sends data to the UART using the UART driver API. The UART echoes back&amp;nbsp;data to the PC.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can refer to MCUXpresso SDK USB stack HOST reference manual for more details.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielchen_0-1655438503541.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183690iA329351C68A55F8C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielchen_0-1655438503541.png" alt="danielchen_0-1655438503541.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielchen_0-1655438503541.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 04:01:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-USB-Host/m-p/1475701#M191581</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-06-17T04:01:54Z</dc:date>
    </item>
  </channel>
</rss>