<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Uboot printing garbage after relocates itself to RAM.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-printing-garbage-after-relocates-itself-to-RAM/m-p/1473701#M191469</link>
    <description>&lt;P&gt;We found out that on new board issues disappear if we enable L1 cache.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Jun 2022 14:15:53 GMT</pubDate>
    <dc:creator>adrian_dusinski</dc:creator>
    <dc:date>2022-06-14T14:15:53Z</dc:date>
    <item>
      <title>Uboot printing garbage after relocates itself to RAM.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-printing-garbage-after-relocates-itself-to-RAM/m-p/1471488#M191322</link>
      <description>&lt;P&gt;We have two custom boards and use single memory 4Gb.&lt;/P&gt;&lt;P&gt;On first board, DDR calibration/stress test passed and uboot log normally.&lt;/P&gt;&lt;P&gt;On second board, calibration and stress test passed, u boot logs correct until relocation to RAM memory occurs.&lt;/P&gt;&lt;P&gt;We checked PCB few times but we can't find issues.&lt;/P&gt;&lt;P&gt;I'm uploading DDR configuration and uboot via JTAG.&lt;/P&gt;&lt;P&gt;Log from working board:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U-Boot 2013.04-rc1 (Jun 09 2022 - 14:18:01)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;CPU: Freescale i.MX6DL rev1.2 at 792 MHz&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Reset cause: POR&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Board: I.MX6DL&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;I2C: ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DRAM: 0 Bytes&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MMC: FSL_SDHC: 0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Card did not respond to voltage select!&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MMC init failed&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Using default environment&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;In: serial&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Out: serial&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Err: serial&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Log from broken board:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U-Boot 2013.04-rc1-Imx6dl (Jun 09 2022 - 14:18:01)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;CPU: Freescale i.MX6DL rev1.2 at 792 MHz&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Reset cause: unknown reset&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Board: Imx6dl&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;I2C: ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DRAM: 0 Bytes&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MMC: FSL_SDHC: 0---------------------------- ! !&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;f!Tesu St`tts&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-------------- ! !&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;f!Tesu St`tts&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;C`re die nou rerpond to vnltafe!seldct!&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MMC init failed&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Using default environment&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;In: serial&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;----ov/&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;-------------- ! !&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;f!Tesu St`tts&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Out: serial&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;----ov/&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;-------------- ! !&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;f!Tesu St`tts&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Err: serial&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;-------------- ! !&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;f!Tesu St`tts&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When uboot use puts function that send data directly to uart, text is okay but if I'm using printf function, text are broken.&lt;/P&gt;&lt;P&gt;Logs from NXP DDR Test tool from broken board:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MMDC0 MPWRDLCTL = 0x40402C32MMDC&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;registers updated from calibration&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Write leveling calibration&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00190019&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x00010001&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Read DQS Gating calibration&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MPDGCTRL0 PHY0 (0x021b083c) = 0x417C0178&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MPDGCTRL1 PHY0 (0x021b0840) = 0x00000000&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Read calibration&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MPRDDLCTL PHY0 (0x021b0848) = 0x40405250&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Write calibration&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MPWRDLCTL PHY0 (0x021b0850) = 0x40402C32&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Success: DDR calibration completed!!!&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DDR Freq: 297 MHz&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t0.1: data is addr test&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t0: memcpy11 SSN test&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t1: memcpy8 SSN test&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t2: byte-wise SSN test&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t3: memcpy11 random pattern test&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t4: IRAM_to_DDRv2 test&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t5: IRAM_to_DDRv1 test&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t6: read noise walking ones and zeros test&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Success: DDR Stress test completed!!!&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know that problem can be in many place but &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;if I can read memory via JTAG it excludes wrong memory connection?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 14:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-printing-garbage-after-relocates-itself-to-RAM/m-p/1471488#M191322</guid>
      <dc:creator>adrian_dusinski</dc:creator>
      <dc:date>2022-06-14T14:14:52Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot printing garbage after relocates itself to RAM.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-printing-garbage-after-relocates-itself-to-RAM/m-p/1473701#M191469</link>
      <description>&lt;P&gt;We found out that on new board issues disappear if we enable L1 cache.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 14:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-printing-garbage-after-relocates-itself-to-RAM/m-p/1473701#M191469</guid>
      <dc:creator>adrian_dusinski</dc:creator>
      <dc:date>2022-06-14T14:15:53Z</dc:date>
    </item>
  </channel>
</rss>