<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic android kernel version change(imx8mqevk) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-kernel-version-change-imx8mqevk/m-p/1473438#M191450</link>
    <description>&lt;P&gt;Hi, I am porting android OS to imx8 processor board now.&lt;/P&gt;&lt;P&gt;Currently, The Android version I am using is Oreo and the kernel version is 4.9.88(imx-o8.1.0_1.3.0)&lt;/P&gt;&lt;P&gt;I want to change the kernel version to 4.14&lt;/P&gt;&lt;P&gt;Because, I have to use SPI.&lt;/P&gt;&lt;P&gt;However, after changing the kernel version and proceeding with the build an error occurred.&lt;/P&gt;&lt;P&gt;"FAILED: out/target /product/evk_8mq/vbmeta.img"&lt;/P&gt;&lt;P&gt;"/bin/bash -c "for dtsplat in imx8mq:fsl-imx8mq-evk.dtb; do DTS_PLATFORM=\`echo \$dtsplat | cut -d':' -f1\`; VBMETA_IMAGE_BOARD=out/target/product/evk_8mq/vbmeta-\$DTS_PLATFORM.img; out/host/linux-x86/bin/avbtool make_vbmeta_image --include_descriptors_from_image out/target/product/evk_8mq/boot-\$DTS_PLATFORM.img --include_descriptors_from_image out/target/product/evk_8mq/system.img --include_descriptors_from_image out/target/product/evk_8mq/vendor.img --algorithm SHA256_RSA4096 --key external/avb/test/data/testkey_rsa4096.pem --padding_size 4096 --output \$VBMETA_IMAGE_BOARD ; done"&lt;BR /&gt;out/host/linux-x86/bin/avbtool: Given image does not look like a vbmeta image.&lt;BR /&gt;ninja: build stopped: subcommand failed."&lt;/P&gt;&lt;P&gt;I wonder why this error occurs???&lt;/P&gt;&lt;P&gt;Thank you!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Jun 2022 07:52:03 GMT</pubDate>
    <dc:creator>dngnstjd</dc:creator>
    <dc:date>2022-06-14T07:52:03Z</dc:date>
    <item>
      <title>android kernel version change(imx8mqevk)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-kernel-version-change-imx8mqevk/m-p/1473438#M191450</link>
      <description>&lt;P&gt;Hi, I am porting android OS to imx8 processor board now.&lt;/P&gt;&lt;P&gt;Currently, The Android version I am using is Oreo and the kernel version is 4.9.88(imx-o8.1.0_1.3.0)&lt;/P&gt;&lt;P&gt;I want to change the kernel version to 4.14&lt;/P&gt;&lt;P&gt;Because, I have to use SPI.&lt;/P&gt;&lt;P&gt;However, after changing the kernel version and proceeding with the build an error occurred.&lt;/P&gt;&lt;P&gt;"FAILED: out/target /product/evk_8mq/vbmeta.img"&lt;/P&gt;&lt;P&gt;"/bin/bash -c "for dtsplat in imx8mq:fsl-imx8mq-evk.dtb; do DTS_PLATFORM=\`echo \$dtsplat | cut -d':' -f1\`; VBMETA_IMAGE_BOARD=out/target/product/evk_8mq/vbmeta-\$DTS_PLATFORM.img; out/host/linux-x86/bin/avbtool make_vbmeta_image --include_descriptors_from_image out/target/product/evk_8mq/boot-\$DTS_PLATFORM.img --include_descriptors_from_image out/target/product/evk_8mq/system.img --include_descriptors_from_image out/target/product/evk_8mq/vendor.img --algorithm SHA256_RSA4096 --key external/avb/test/data/testkey_rsa4096.pem --padding_size 4096 --output \$VBMETA_IMAGE_BOARD ; done"&lt;BR /&gt;out/host/linux-x86/bin/avbtool: Given image does not look like a vbmeta image.&lt;BR /&gt;ninja: build stopped: subcommand failed."&lt;/P&gt;&lt;P&gt;I wonder why this error occurs???&lt;/P&gt;&lt;P&gt;Thank you!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 07:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-kernel-version-change-imx8mqevk/m-p/1473438#M191450</guid>
      <dc:creator>dngnstjd</dc:creator>
      <dc:date>2022-06-14T07:52:03Z</dc:date>
    </item>
    <item>
      <title>Re: android kernel version change(imx8mqevk)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-kernel-version-change-imx8mqevk/m-p/1473732#M191471</link>
      <description>&lt;P&gt;Hello dngnstjd,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You have to adjust and compile the device tree at 4.14v, since you are changing kernel version.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 14:52:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-kernel-version-change-imx8mqevk/m-p/1473732#M191471</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-06-14T14:52:54Z</dc:date>
    </item>
  </channel>
</rss>