<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using iMX8M Mini UART 3 for M4 as a Bluetooth interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-iMX8M-Mini-UART-3-for-M4-as-a-Bluetooth-interface/m-p/1473162#M191424</link>
    <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please note that support for zephyr is community based, not direct from NXP. I'll recommend for issue using zephyr in the i.MX MPUs post them at zephyr community.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Mon, 13 Jun 2022 22:00:45 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2022-06-13T22:00:45Z</dc:date>
    <item>
      <title>Using iMX8M Mini UART 3 for M4 as a Bluetooth interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-iMX8M-Mini-UART-3-for-M4-as-a-Bluetooth-interface/m-p/1471337#M191315</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to use&amp;nbsp;iMX8M Mini, UART 3 for M4 as a Bluetooth interface. M4 will be running with Zephyr OS.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;On the EVK board UART3 is available from the header and the p&lt;/SPAN&gt;&lt;SPAN&gt;in details for UART 3&lt;BR /&gt;TXD &amp;nbsp; - &amp;nbsp; Pin 8&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;RXD&amp;nbsp;&amp;nbsp; - &amp;nbsp; Pin 10&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In Zephyr (boards/arm/mimx8mm_evk/mimx8mm_evk.dts) I have modified the device tree like below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;zephyr,bt-uart = &amp;amp;uart3;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;amp;uart3 {&lt;BR /&gt;status = "okay";&lt;BR /&gt;current-speed = &amp;lt;115200&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Do I need to do any other changes? What about RDC domain settings?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does&amp;nbsp; M4 needs to be in RDC domain 1 and&amp;nbsp;UART3 needs to be assigned to domain 1 ? Where this changes are needed? Is it in Zephyr or in the u-boot?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Any help is appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance,&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Pradeep&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jun 2022 09:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-iMX8M-Mini-UART-3-for-M4-as-a-Bluetooth-interface/m-p/1471337#M191315</guid>
      <dc:creator>pradeep2481</dc:creator>
      <dc:date>2022-06-09T09:00:36Z</dc:date>
    </item>
    <item>
      <title>Re: Using iMX8M Mini UART 3 for M4 as a Bluetooth interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-iMX8M-Mini-UART-3-for-M4-as-a-Bluetooth-interface/m-p/1473162#M191424</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please note that support for zephyr is community based, not direct from NXP. I'll recommend for issue using zephyr in the i.MX MPUs post them at zephyr community.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jun 2022 22:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-iMX8M-Mini-UART-3-for-M4-as-a-Bluetooth-interface/m-p/1473162#M191424</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-06-13T22:00:45Z</dc:date>
    </item>
  </channel>
</rss>