<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMXRT1024 DCP CRC-32 parameter settings in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMXRT1024-DCP-CRC-32-parameter-settings/m-p/1472829#M191411</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the i.MX RT1024 evaluation board and trying to use the CRC32 to verify some data.&lt;/P&gt;&lt;P&gt;I used the dcp example without problem but when I tried to use the verify with an old data the result is not as expected cause of the settings.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CRC32 included in the example use the parameters showns below:&lt;/P&gt;&lt;P&gt;width=32 poly=0x04c11db7 init=0xffffffff refin=false refout=false xorout=0x00000000&lt;/P&gt;&lt;P&gt;I know that these parameters are for CRC-32/MPEG-2 but&amp;nbsp;my parameters are not exactly the same that these.&lt;/P&gt;&lt;P&gt;Is it possible to change these parameters?&lt;/P&gt;</description>
    <pubDate>Mon, 13 Jun 2022 11:01:18 GMT</pubDate>
    <dc:creator>JasonGT93</dc:creator>
    <dc:date>2022-06-13T11:01:18Z</dc:date>
    <item>
      <title>iMXRT1024 DCP CRC-32 parameter settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMXRT1024-DCP-CRC-32-parameter-settings/m-p/1472829#M191411</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the i.MX RT1024 evaluation board and trying to use the CRC32 to verify some data.&lt;/P&gt;&lt;P&gt;I used the dcp example without problem but when I tried to use the verify with an old data the result is not as expected cause of the settings.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The CRC32 included in the example use the parameters showns below:&lt;/P&gt;&lt;P&gt;width=32 poly=0x04c11db7 init=0xffffffff refin=false refout=false xorout=0x00000000&lt;/P&gt;&lt;P&gt;I know that these parameters are for CRC-32/MPEG-2 but&amp;nbsp;my parameters are not exactly the same that these.&lt;/P&gt;&lt;P&gt;Is it possible to change these parameters?&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jun 2022 11:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMXRT1024-DCP-CRC-32-parameter-settings/m-p/1472829#M191411</guid>
      <dc:creator>JasonGT93</dc:creator>
      <dc:date>2022-06-13T11:01:18Z</dc:date>
    </item>
    <item>
      <title>Re: iMXRT1024 DCP CRC-32 parameter settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMXRT1024-DCP-CRC-32-parameter-settings/m-p/1475166#M191552</link>
      <description>&lt;P&gt;Could anyone contribute?&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 08:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMXRT1024-DCP-CRC-32-parameter-settings/m-p/1475166#M191552</guid>
      <dc:creator>JasonGT93</dc:creator>
      <dc:date>2022-06-16T08:42:56Z</dc:date>
    </item>
    <item>
      <title>Re: iMXRT1024 DCP CRC-32 parameter settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMXRT1024-DCP-CRC-32-parameter-settings/m-p/1490740#M192639</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201400"&gt;@JasonGT93&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope that you are doing great!&lt;/P&gt;
&lt;P&gt;After checking , I am able to confirm that the RT1020 DCP do not have a provision to change CRC-32 parameters. So you can only compute for CRC32-MPEG-2.&lt;/P&gt;
&lt;P&gt;I am sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;Let me know if there is anything else to discuss.&lt;/P&gt;
&lt;P&gt;All the best,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 05:11:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMXRT1024-DCP-CRC-32-parameter-settings/m-p/1490740#M192639</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2022-07-18T05:11:59Z</dc:date>
    </item>
  </channel>
</rss>