<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-Driver-for-NXP-i-MX8MP-supporting-FreeRTOS-CortexM-7/m-p/1472258#M191366</link>
    <description>&lt;P&gt;Does NXP provide the&amp;nbsp;Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)?&lt;/P&gt;&lt;P&gt;The variscite board var-som-mx8mp board has both the ethernets made available for the Cortex A-53 ( OS: Linux), I need to use one of the ethernet for Cortex M-7 ( OS: FreeRTOS).&lt;/P&gt;&lt;P&gt;Can anyone help me find the driver for the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 10 Jun 2022 13:15:45 GMT</pubDate>
    <dc:creator>Samhitha_Kashyap</dc:creator>
    <dc:date>2022-06-10T13:15:45Z</dc:date>
    <item>
      <title>Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-Driver-for-NXP-i-MX8MP-supporting-FreeRTOS-CortexM-7/m-p/1472258#M191366</link>
      <description>&lt;P&gt;Does NXP provide the&amp;nbsp;Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)?&lt;/P&gt;&lt;P&gt;The variscite board var-som-mx8mp board has both the ethernets made available for the Cortex A-53 ( OS: Linux), I need to use one of the ethernet for Cortex M-7 ( OS: FreeRTOS).&lt;/P&gt;&lt;P&gt;Can anyone help me find the driver for the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jun 2022 13:15:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-Driver-for-NXP-i-MX8MP-supporting-FreeRTOS-CortexM-7/m-p/1472258#M191366</guid>
      <dc:creator>Samhitha_Kashyap</dc:creator>
      <dc:date>2022-06-10T13:15:45Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Ethernet-Driver-for-NXP-i-MX8MP-supporting-FreeRTOS-CortexM-7/m-p/1473068#M191421</link>
      <description>&lt;P&gt;Hello, &lt;BR /&gt;&lt;BR /&gt;The Cortex-M Core are mainly intended for real-time application, delegating the high-speed communications (like ethernet and USB) to the Cortex-A cores.&lt;/P&gt;
&lt;P&gt;With the above into account we do not provide an ethernet driver for the Cortex M7. &lt;BR /&gt;&lt;BR /&gt;Best regards, &lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jun 2022 18:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Ethernet-Driver-for-NXP-i-MX8MP-supporting-FreeRTOS-CortexM-7/m-p/1473068#M191421</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2022-06-13T18:39:29Z</dc:date>
    </item>
  </channel>
</rss>