<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: USB OTG to USB HOST</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237543#M19135</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Could you clarify why this is not possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe I should clarify my needs. I'm building a system that will need two host connectors. I also want to use MFGTool in production. What would be the best way to solve this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Feb 2014 07:15:08 GMT</pubDate>
    <dc:creator>emil</dc:creator>
    <dc:date>2014-02-17T07:15:08Z</dc:date>
    <item>
      <title>USB OTG to USB HOST</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237541#M19133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on a iMX6 system that needs two USB 2.0 hosts and one OTG port for MFGTool. MFGTool is the only reason for OTG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to just use the OTG transciever as a 2.0 Host by grounding the ID pin? Does the MFGTool assume that the PC supplies VBUS, or could I connect a regular standard-A connector to the PC and still have ID pin grounded on iMX6 side (i.e iMX6 supplies VBUS)? Or does MFGTool/iMX6 assume that VBUS is supplied from PC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2014 18:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237541#M19133</guid>
      <dc:creator>emil</dc:creator>
      <dc:date>2014-02-14T18:26:22Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG to USB HOST</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237542#M19134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,emil,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I can understand your meaning, but I don't recommend you operate USB OTG like what you described.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. USB OTG works as a device&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;USB_OTG_ID pin should be pulled down to HIGH&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2. USB_OTG works as a host&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;USB_OTG_ID pin should be&amp;nbsp; pulled down to LOW&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3. Designing USB OTG works as dual role&lt;/STRONG&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you want USB OTG to not only works as device,but also host, you can design it to be dual role. there are 2 ways to realize it on your board.&lt;/P&gt;&lt;P&gt;(1)Only use one microUSB connector.&lt;/P&gt;&lt;P&gt;(2)Using MicroUSB connector for device role, and using USB Host connector for host interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2014 06:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237542#M19134</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2014-02-17T06:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG to USB HOST</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237543#M19135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Could you clarify why this is not possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe I should clarify my needs. I'm building a system that will need two host connectors. I also want to use MFGTool in production. What would be the best way to solve this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2014 07:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237543#M19135</guid>
      <dc:creator>emil</dc:creator>
      <dc:date>2014-02-17T07:15:08Z</dc:date>
    </item>
    <item>
      <title>Re: Re: USB OTG to USB HOST</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237544#M19136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, emil,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; USB OTG ID is used to determine the role of USB OTG. The high level on USB_OTG_PIN means USB OTG works as a device, and low level means it works as a host. So if you wants it works a dual role, you have 2 ways to design USB OTG circuit.&lt;/P&gt;&lt;P&gt;(1) Only using one microUSB connector.&lt;/P&gt;&lt;P&gt;Please refter to i.mx51 evaluation board !&lt;/P&gt;&lt;P&gt;(2) Using one microUSB connector for device, and Using a USB HOST connector for USB Host.&lt;/P&gt;&lt;P&gt;Please refer to i.mx53 QSB evaluation board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can refter above 2 schematic, and select one usage for your USB OTG design of i.mx6 product.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; See attachment ! SPF-26203_C3.pdf is the schematic of i.mx51 evk, the other is that of i.mx53QSB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In addition, MFG Tools requires USB OTG on your board should work as a device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2014 06:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237544#M19136</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2014-02-24T06:15:50Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG to USB HOST</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237545#M19137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Email&lt;/P&gt;&lt;P&gt;Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2014 08:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237545#M19137</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-03-21T08:08:26Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG to USB HOST</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237546#M19138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Email&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2014 07:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-to-USB-HOST/m-p/237546#M19138</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-04-01T07:09:22Z</dc:date>
    </item>
  </channel>
</rss>