<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX7D SDMA data transfer stop immediately? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-SDMA-data-transfer-stop-immediately/m-p/1471357#M191316</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to transfer the output result converted by ADC to the memory by SDMA.&lt;BR /&gt;Set the Channel Stop / Channel Status (SDMAARM_STOP_STAT) bit to stop data transfer&lt;BR /&gt;The ADC peripheral clock has stopped.&lt;BR /&gt;Then, in rare cases, it seems that an abort exception occurs when transferring data.&lt;BR /&gt;I think this is because the ADC was accessed because the SDMA data transfer did not stop immediately.&lt;BR /&gt;Is it necessary to stop the data transfer and then wait?&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jun 2022 09:28:30 GMT</pubDate>
    <dc:creator>akihiro_kimura</dc:creator>
    <dc:date>2022-06-09T09:28:30Z</dc:date>
    <item>
      <title>iMX7D SDMA data transfer stop immediately?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX7D-SDMA-data-transfer-stop-immediately/m-p/1471357#M191316</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to transfer the output result converted by ADC to the memory by SDMA.&lt;BR /&gt;Set the Channel Stop / Channel Status (SDMAARM_STOP_STAT) bit to stop data transfer&lt;BR /&gt;The ADC peripheral clock has stopped.&lt;BR /&gt;Then, in rare cases, it seems that an abort exception occurs when transferring data.&lt;BR /&gt;I think this is because the ADC was accessed because the SDMA data transfer did not stop immediately.&lt;BR /&gt;Is it necessary to stop the data transfer and then wait?&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jun 2022 09:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX7D-SDMA-data-transfer-stop-immediately/m-p/1471357#M191316</guid>
      <dc:creator>akihiro_kimura</dc:creator>
      <dc:date>2022-06-09T09:28:30Z</dc:date>
    </item>
  </channel>
</rss>