<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX535 Custom Platform - Code Hang</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX535-Custom-Platform-Code-Hang/m-p/237478#M19116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: This issue is resolved now. The issue was with respect to the DDR calibraion.&lt;/P&gt;&lt;P&gt;The DDR relevant read &amp;amp; write delay lines were tuned to get the stress test working till 400MHz in our hardware platform.&lt;/P&gt;&lt;P&gt;After this update no code hang occurs.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 13 Jul 2013 09:01:45 GMT</pubDate>
    <dc:creator>SrideviK</dc:creator>
    <dc:date>2013-07-13T09:01:45Z</dc:date>
    <item>
      <title>i.MX535 Custom Platform - Code Hang</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX535-Custom-Platform-Code-Hang/m-p/237477#M19115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have our custom design based on i.MX535 SMD design with 512MB LPDDR2-S4 &amp;amp; 4GB eMMC Flash. The reference BSP details&amp;nbsp; taken for customization is given below.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;Reference BSP&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Patches taken from R10.4 Freescale Release&lt;/P&gt;&lt;P&gt;Uboot 2009.08&lt;/P&gt;&lt;P&gt;Android 2.3.7 Sabre Tablet BSP (Linux Kernel 2.6.35)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have made the bootstraps for Micro-SD booting &amp;amp; have the Micro-SD card with all the images in the respective partitions.&lt;/P&gt;&lt;P&gt;One of the hardware is functioning ok with the Micro-SD booting and the BSP loading &amp;amp; execution is all fine in this hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in the second hardware platform, with the same set of images in Micro-SD, only the U-boot booting &amp;amp; execution is ok all the time. Kernel loading is always ok.&lt;/P&gt;&lt;P&gt;The following inconsistency exists in terms of the observations / results as follows:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; But code execution hangs most of the time showing "Starting kernel...".&lt;/P&gt;&lt;P&gt;2. Sometimes, even the kernel execution is initiated but code hangs showing kernel panic at different points.&lt;/P&gt;&lt;P&gt;3. Tried TFTP in U-boot to isolate the Micro-SD dependency. The code loading happens. But code execution hangs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The above observation or code hang does not happen at any specific point to help backtracing. It is very random.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: &lt;/P&gt;&lt;P&gt;But the second hardware platform is tested ok for the following:&lt;/P&gt;&lt;P&gt;(a) Micro-SD booting. Uboot booting is always fine.&lt;/P&gt;&lt;P&gt;(b) Micro-SD card access (Read/write via U-boot)&lt;/P&gt;&lt;P&gt;(c) DDR Stress Test upto 333MHz DDR frequency (for which the hardware configuration is made)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pls advice how to address this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward for your earliest support.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sridevi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jun 2013 06:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX535-Custom-Platform-Code-Hang/m-p/237477#M19115</guid>
      <dc:creator>SrideviK</dc:creator>
      <dc:date>2013-06-25T06:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX535 Custom Platform - Code Hang</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX535-Custom-Platform-Code-Hang/m-p/237478#M19116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: This issue is resolved now. The issue was with respect to the DDR calibraion.&lt;/P&gt;&lt;P&gt;The DDR relevant read &amp;amp; write delay lines were tuned to get the stress test working till 400MHz in our hardware platform.&lt;/P&gt;&lt;P&gt;After this update no code hang occurs.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jul 2013 09:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX535-Custom-Platform-Code-Hang/m-p/237478#M19116</guid>
      <dc:creator>SrideviK</dc:creator>
      <dc:date>2013-07-13T09:01:45Z</dc:date>
    </item>
  </channel>
</rss>