<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: LPUART pins</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1468471#M191130</link>
    <description>&lt;P&gt;Hello &lt;BR /&gt;Hope you are well.&lt;BR /&gt;Could you please provide me the part number you are using? This to confirm&amp;nbsp; if LPUART3 is present on those pins.&lt;/P&gt;
&lt;P&gt;If EMC bank is 1.8v, the output from those pins will be 1.8v while the GPIO_AD bank output will be 3.3v. This could cause issues depending on the operating voltage of the device you´re trying to communicate.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jun 2022 23:26:28 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2022-06-02T23:26:28Z</dc:date>
    <item>
      <title>LPUART pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1466888#M191017</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can&amp;nbsp;&lt;SPAN class=""&gt;LPUART3 work using the following pins?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;LPUART3_TXD- GPIO_B0_08&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;LPUART3_RXD-&amp;nbsp;GPIO_EMC_14&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;LPUART3_CTS_B-&amp;nbsp;GPIO_AD_B1_04&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;LPUART3_RTS_B-&amp;nbsp;GPIO_EMC_16&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;In case yes, what will happen when the EMC bank is 1.8v and the GPIO bank is 3.3V?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 31 May 2022 15:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1466888#M191017</guid>
      <dc:creator>sapirbuz</dc:creator>
      <dc:date>2022-05-31T15:16:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1468471#M191130</link>
      <description>&lt;P&gt;Hello &lt;BR /&gt;Hope you are well.&lt;BR /&gt;Could you please provide me the part number you are using? This to confirm&amp;nbsp; if LPUART3 is present on those pins.&lt;/P&gt;
&lt;P&gt;If EMC bank is 1.8v, the output from those pins will be 1.8v while the GPIO_AD bank output will be 3.3v. This could cause issues depending on the operating voltage of the device you´re trying to communicate.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jun 2022 23:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1468471#M191130</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-06-02T23:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1469283#M191185</link>
      <description>&lt;P&gt;thank you &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;the PN is MIMXRT1051CVL5B&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jun 2022 09:44:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1469283#M191185</guid>
      <dc:creator>sapirbuz</dc:creator>
      <dc:date>2022-06-06T09:44:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1469556#M191199</link>
      <description>&lt;P&gt;Thank you. Those pins have LPUART functionality and can be used.&amp;nbsp; Please consider that powering the rails with different voltages will have different output voltages in each pin.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jun 2022 23:05:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1469556#M191199</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2022-06-06T23:05:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1469779#M191211</link>
      <description>&lt;P&gt;thank you &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 07:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LPUART-pins/m-p/1469779#M191211</guid>
      <dc:creator>sapirbuz</dc:creator>
      <dc:date>2022-06-07T07:11:27Z</dc:date>
    </item>
  </channel>
</rss>