<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 imx6ull: NAND writes from uboot makes read errors from Linux and vice-versa</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-NAND-writes-from-uboot-makes-read-errors-from-Linux-and/m-p/1467812#M191077</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to create and write my NAND volumes from uboot.&lt;/P&gt;&lt;P&gt;The board is the imx6ull-colibri from Toradex. uboot and kernel are mainline.&lt;/P&gt;&lt;P&gt;But when I do so, I have ECC error from linux, when performing the "ubiattach" command.&lt;/P&gt;&lt;P&gt;Similarly, when creating the volumes from linux, there are ECC errors when reading them&lt;/P&gt;&lt;P&gt;in u-boot.&lt;/P&gt;&lt;P&gt;I have tried to change the device tree (as suggested on other platforms with simular issues) as such:&lt;/P&gt;&lt;P&gt;nand-ecc-mode = "hw"; to "on-die", with no better success, as well as adding "fsl,use-minimum-ecc"&lt;/P&gt;&lt;P&gt;In some past threads on NXP forums, it was said that writing the NAND was only supported from linux, is this still the case today ?&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jun 2022 06:30:10 GMT</pubDate>
    <dc:creator>tbultel</dc:creator>
    <dc:date>2022-06-02T06:30:10Z</dc:date>
    <item>
      <title>imx6ull: NAND writes from uboot makes read errors from Linux and vice-versa</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-NAND-writes-from-uboot-makes-read-errors-from-Linux-and/m-p/1467812#M191077</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I would like to create and write my NAND volumes from uboot.&lt;/P&gt;&lt;P&gt;The board is the imx6ull-colibri from Toradex. uboot and kernel are mainline.&lt;/P&gt;&lt;P&gt;But when I do so, I have ECC error from linux, when performing the "ubiattach" command.&lt;/P&gt;&lt;P&gt;Similarly, when creating the volumes from linux, there are ECC errors when reading them&lt;/P&gt;&lt;P&gt;in u-boot.&lt;/P&gt;&lt;P&gt;I have tried to change the device tree (as suggested on other platforms with simular issues) as such:&lt;/P&gt;&lt;P&gt;nand-ecc-mode = "hw"; to "on-die", with no better success, as well as adding "fsl,use-minimum-ecc"&lt;/P&gt;&lt;P&gt;In some past threads on NXP forums, it was said that writing the NAND was only supported from linux, is this still the case today ?&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jun 2022 06:30:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-NAND-writes-from-uboot-makes-read-errors-from-Linux-and/m-p/1467812#M191077</guid>
      <dc:creator>tbultel</dc:creator>
      <dc:date>2022-06-02T06:30:10Z</dc:date>
    </item>
  </channel>
</rss>